This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-5 [12 Jul 2019 13:02] – Pop Andreea | university:courses:electronics:electronics-lab-5 [23 Aug 2019 12:40] – Antoniu Miclaus | ||
---|---|---|---|
Line 25: | Line 25: | ||
<WRAP centeralign> | <WRAP centeralign> | ||
- | The waveform generator output W1 should be configured for a 1 KHz sine wave with 3 volt amplitude and 0 volt offset. The setup should be configured with scope channel 1+ connected to display the output W1. Scope channel 2 (2+) is used to measure alternately the waveform at the base and collector of Q< | + | The waveform generator output W1 should be configured for a 1 KHz sine wave with 3 volt amplitude |
===== Procedure: ===== | ===== Procedure: ===== |