This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-4m [25 Jun 2020 22:07] – external edit | university:courses:electronics:electronics-lab-4m [22 Jul 2020 11:25] – [Procedure:] Figure 3 Replaced Vds with Vgs Pop Andreea | ||
---|---|---|---|
Line 25: | Line 25: | ||
<WRAP centeralign> | <WRAP centeralign> | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
The arbitrary waveform generator should be configured for a 100 Hz triangle wave with 2.5 volt amplitude peak-to-peak and 1.25 volt offset. The differential scope channel 2 (2+/-) measures the current in the resistor (and in the transistor). Scope channel 1 should be connected to display the output of the waveform generator. The current flowing through the transistor is the voltage difference 2+ and 2- divided by the resistor value (100Ω). | The arbitrary waveform generator should be configured for a 100 Hz triangle wave with 2.5 volt amplitude peak-to-peak and 1.25 volt offset. The differential scope channel 2 (2+/-) measures the current in the resistor (and in the transistor). Scope channel 1 should be connected to display the output of the waveform generator. The current flowing through the transistor is the voltage difference 2+ and 2- divided by the resistor value (100Ω). | ||
Line 34: | Line 34: | ||
<WRAP centeralign> | <WRAP centeralign> | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
Load the captured data in to Excel and calculate the current. Plot the drain current vs. the gate voltage of the transistor (V< | Load the captured data in to Excel and calculate the current. Plot the drain current vs. the gate voltage of the transistor (V< |