This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-4m [12 Jul 2019 13:01] – [Activity 4M. NMOS FET characteristic curves] Pop Andreea | university:courses:electronics:electronics-lab-4m [23 Aug 2019 12:39] – Antoniu Miclaus | ||
---|---|---|---|
Line 27: | Line 27: | ||
<WRAP centeralign> | <WRAP centeralign> | ||
- | The arbitrary waveform generator should be configured for a 100 Hz triangle wave with 2.5 volt amplitude and 1.25 volt offset. The differential scope channel 2 (2+/-) measures the current in the resistor (and in the transistor). Scope channel 1 should be connected to display the output of the waveform generator. The current flowing through the transistor is the voltage difference 2+ and 2- divided by the resistor value (100Ω). | + | The arbitrary waveform generator should be configured for a 100 Hz triangle wave with 2.5 volt amplitude |
Line 69: | Line 69: | ||
The setup is the same as the previous experiment except now Scope channel 1 is set to display the transistor V< | The setup is the same as the previous experiment except now Scope channel 1 is set to display the transistor V< | ||
- | A stair-step waveform will be needed to drive the gate of the transistor. Using the buffer in the Scopy Signal Generator tool, construct a stair-step waveform with 5 levels on channel 2 (W2). Load the following csv file (extract from archive): {{: | + | A stair-step waveform will be needed to drive the gate of the transistor. Using the buffer in the Scopy Signal Generator tool, construct a stair-step waveform with 5 levels on channel 2 (W2). Load the following csv file (extract from archive): {{: |
===== Procedure: ===== | ===== Procedure: ===== |