Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision |
university:courses:electronics:electronics-lab-4 [07 Nov 2018 09:17] – Updated the breadboard connections as well as the Scopy plot. Changed the phase from 270 degrees to 90 to follow the set-up in Scopy as what the direction has stated. Interchanged the positions of 1+ and 1- to correctly plot the IE vs VBE Scopy plot. Chan Hannah Rosete | university:courses:electronics:electronics-lab-4 [03 Jan 2021 22:12] – fix links Robin Getz |
---|
====== Activity 4. A BJT Curve Tracer ====== | ====== Activity: A BJT Curve Tracer ====== |
| |
===== Objective: ===== | ===== Objective: ===== |
===== Directions and Setup: ===== | ===== Directions and Setup: ===== |
| |
Build the simple curve tracer circuit shown in figure 1. The green boxes indicate where to connect the ADALM2000. Using the custom waveform editor in the Scopy AWG tool, construct a stair-step waveform with 5 levels. Be sure to reset so that you are starting with flat line at 0%. First set the type to constant. Then with start set to 0%, length set to 20% and offset set to -100% click on generate function. There should now be a line at -100% from 0 to 20%. Next change the start to 20% and the offset to -50% and then click on generate function again. There should now be a line at -50% from 20% to 40%. Next set the offset to +50% and the start to 60% and then click on generate function again. There should now be a line at 0% from 40% to 60% and a line at 50% from 60% to 80%. Finally set the offset to 100% and start to 80% and click on generate function one last time. There should now be a final line at 100% from 80% to 100%. Click on save and your new waveform should be in channel 2. Now at this point set the frequency to 40Hz, the amplitude to 2 V and the offset to 2.6 V. The waveform in the display should start at 0.6V and increase in 1 V increments to 4.6 V (0.6, 1.6, 2.6, 3.6, 4.6) Each step should be 5 mSec long for a total of 25 mSec. In AWG channel 1 configure a triangle wave with an amplitude of 2.5 V and an offset of 2.5V (wave should swing from 0 to 5V). Set the frequency to 200 Hz ( 5 times the 40 Hz of channel 2). Comparing the waveforms in channel 1 and channel 2, the triangle wave in channel 1 should go through one cycle from 0 to 5 V and back to zero during the time of one step in the waveform in channel 2. It will probably be necessary to set the phase of channel 1 to 90 degrees to make them line up in this way. | Build the simple curve tracer circuit shown in Figure 1. The green boxes indicate where to connect the ADALM2000. Using the Scopy Signal Generator tool, in Channel 2 Buffer tab import the csv file for the stairstep signal needed. |
| Now at this point set the amplitude to 2 V peak-to-peak and the offset to 2.6 V. The waveform in the display should start at 0.6V and increase in 1 V increments to 4.6 V (0.6, 1.6, 2.6, 3.6, 4.6). For each step to be 5 mSec long for a total of 25 mSec, set the sampling rate 200 Hz. |
| In Signal Generator Channel 1 configure a triangle wave with an amplitude of 5V peak-to-peak and an offset of 2.5V (wave should swing from 0 to 5V). Set the frequency to 200 Hz ( 5 times the 40 Hz of channel 2). Comparing the waveforms in Channel 1 and Channel 2, the triangle wave in Channel 1 should go through one cycle from 0 to 5 V and back to zero during the time of one step in the waveform in Channel 2. It will probably be necessary to set the phase of Channel 1 to 90 degrees to make them line up in this way. |
| |
You should export your newly created stair-step waveform to a .csv file for future use. | |
| |
===== Procedure: ===== | ===== Procedure: ===== |
<WRAP centeralign> Figure 15, Circuit to measure V<sub>BE</sub> breadboard connection </WRAP> | <WRAP centeralign> Figure 15, Circuit to measure V<sub>BE</sub> breadboard connection </WRAP> |
| |
The generator output W1 should be configured for a 100 Hz triangle wave with 2 volt amplitude and -2 volt offset (for an NPN device). The single ended input of scope channel 2+ is used to measure the voltage at the base of the transistor (optionally connect 2- to the emitter to remove any input offset of the op-amp). The setup should be configured with channel 1 connected to display the output of W1 and channel 2 connected to display the base voltage. The emitter current is calculated as the voltage of W1 / 1KΩ. | The generator output W1 should be configured for a 100 Hz triangle wave with 2 volt amplitude peak-to-peak and -2 volt offset (for an NPN device). The single ended input of scope channel 2+ is used to measure the voltage at the base of the transistor (optionally connect 2- to the emitter to remove any input offset of the op-amp). The setup should be configured with channel 1 connected to display the output of W1 and channel 2 connected to display the base voltage. The emitter current is calculated as the voltage of W1 / 1KΩ. |
| |
===== Procedure: ===== | ===== Procedure: ===== |
This same circuit can be used to measure PNP devices by simply configuring the ramp signal to be positive, i.e. from 0V to the maximum positive swing of the source. | This same circuit can be used to measure PNP devices by simply configuring the ramp signal to be positive, i.e. from 0V to the maximum positive swing of the source. |
| |
| <WRAP round download> |
| ** Lab Resources:** |
| * Fritzing files: [[downgit>education_tools/tree/master/m2k/fritzing/bjt_curve_bb | bjt_curve_bb]] |
| * LTSpice files: [[downgit>education_tools/tree/master/m2k/ltspice/bjt_curve_ltspice | bjt_curve_ltspice]] |
| * Stairstep signal: [[downgit>education_tools/blob/master/m2k/import_waveforms/waveforms_sg/stairstep.csv | stairstep]] |
| </WRAP> |
==== For further reading on the Howland current source: ==== | ==== For further reading on the Howland current source: ==== |
| |
[[http://www.cirrus.com/en/pubs/whitePaper/199210-Apex-Versatile_current_source_circuits.pdf|http://www.cirrus.com/en/pubs/whitePaper/199210-Apex-Versatile_current_source_circuits.pdf]] | [[http://www.cirrus.com/en/pubs/whitePaper/199210-Apex-Versatile_current_source_circuits.pdf|http://www.cirrus.com/en/pubs/whitePaper/199210-Apex-Versatile_current_source_circuits.pdf]] |
| |
[[http://www.analog.com/static/imported-files/application_notes/236037846AN_843.pdf|http://www.analog.com/static/imported-files/application_notes/236037846AN_843.pdf]] | [[adi>static/imported-files/application_notes/236037846AN_843.pdf|http://www.analog.com/static/imported-files/application_notes/236037846AN_843.pdf]] |
| |
[[http://michaelgellis.tripod.com/howland.html|http://michaelgellis.tripod.com/howland.html]] | [[http://michaelgellis.tripod.com/howland.html|http://michaelgellis.tripod.com/howland.html]] |