Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
university:courses:electronics:electronics-lab-3 [23 Jan 2020 21:08]
Doug Mercer [Hardware Setup:]
university:courses:electronics:electronics-lab-3 [23 Jan 2020 21:23]
Doug Mercer [Directions:]
Line 93: Line 93:
 ===== Directions: ===== ===== Directions: =====
  
-Set up the breadboard with waveform generator W1 attached to one end of the series connected resistor R<​sub>​1</​sub>​ and collector of NPN Q<​sub>​1</​sub>​ and the base of PNP Q<​sub>​2</​sub>​ as shown in the diagram. The emitter of Q<​sub>​1</​sub>​ is connected to ground. The collector of Q<​sub>​2</​sub>​is connected to Vn (5V). The first end of Resistor R<​sub>​2</​sub>​ is connected to Vp (5V). The second end of R<​sub>​2</​sub>​ is connected to the base of Q<​sub>​1</​sub>​ and the emitter of Q<​sub>​2</​sub>​. Single ended input of scope channel 2 (2+) is connected to the collector of Q<​sub>​1</​sub>​.+Set up the breadboard with waveform generator W1 attached to one end of the series connected resistor R<​sub>​1</​sub>​ and collector of NPN Q<​sub>​1</​sub>​ and the base of PNP Q<​sub>​2</​sub>​ as shown in the diagram. The emitter of Q<​sub>​1</​sub>​ is connected to ground. The collector of Q<​sub>​2</​sub>​is connected to Vn (-5V). The first end of Resistor R<​sub>​2</​sub>​ is connected to Vp (+5V). The second end of R<​sub>​2</​sub>​ is connected to the base of Q<​sub>​1</​sub>​ and the emitter of Q<​sub>​2</​sub>​. Single ended input of scope channel 2 (2+) is connected to the collector of Q<​sub>​1</​sub>​.
  
 {{ :​university:​courses:​electronics:​a3_f3.png?​500 |}} {{ :​university:​courses:​electronics:​a3_f3.png?​500 |}}
university/courses/electronics/electronics-lab-3.txt · Last modified: 25 Jun 2020 22:07 (external edit)