This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-3 [05 Mar 2019 11:03] – [Procedure:] Antoniu Miclaus | university:courses:electronics:electronics-lab-3 [23 Aug 2019 12:14] – Antoniu Miclaus | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== Activity | + | ====== Activity: The BJT connected as a diode ===== |
===== Objective: ===== | ===== Objective: ===== | ||
Line 21: | Line 21: | ||
===== Hardware Setup: ===== | ===== Hardware Setup: ===== | ||
- | The waveform generator should be configured for a 100 Hz triangle wave with 6 volt amplitude and 0 offset. The differential scope channel 2 (2+, 2-) measures the current in the resistor (and in the transistor). Scope channel 1 (1+) is connected to measure the voltage across the transistor. The current flowing through the transistor, is the voltage difference 1+ and 1- divided by the resistor value (1KΩ). | + | The waveform generator should be configured for a 100 Hz triangle wave with 6 volt amplitude |
{{ : | {{ : | ||
Line 58: | Line 58: | ||
===== Hardware Setup: ===== | ===== Hardware Setup: ===== | ||
- | The waveform generator should be configured for a 100 Hz triangle wave with 10 volt amplitude and 0 volt offset. Scope channel 1 (1+) is used to measure the voltage across the transistor. The setup should be configured with channel 2 connected across resistor R< | + | The waveform generator should be configured for a 100 Hz triangle wave with 10 volt amplitude |
{{ : | {{ : | ||
Line 101: | Line 101: | ||
===== Hardware Setup: ===== | ===== Hardware Setup: ===== | ||
- | The waveform generator should be configured for a 100 Hz triangle wave with 8 volt amplitude and 2 volt offset. Scope channel 2 (2+) is used to measure the voltage across the transistor. The current flowing through the transistor, is the voltage difference between scope input 1+ and 1- divided by the resistor value (1K?). | + | The waveform generator should be configured for a 100 Hz triangle wave with 8 volt amplitude |
{{ : | {{ : | ||
Line 141: | Line 141: | ||
===== Hardware Setup: ===== | ===== Hardware Setup: ===== | ||
- | The waveform generator should be configured for a 100 Hz triangle wave with 4 volt amplitude and 2V offset. The Single ended input of scope channel 2+ is used to measure the voltage across the transistor. The setup should be configured with channel 1+ connected to display the output of generator W1 and channel 2+ connected to display the collector voltage of Q< | + | The waveform generator should be configured for a 100 Hz triangle wave with 4 volt amplitude |
{{ : | {{ : |