university:courses:electronics:electronics-lab-32 [05 Mar 2019 12:34]
Antoniu Miclaus [Other uses for this circuit:]
university:courses:electronics:electronics-lab-32 [25 Jun 2020 22:07] (current)
Line 61: Line 61:
 =====Hardware Setup:===== =====Hardware Setup:=====
  
-AWG1 is connected as V<​sub>​IN</​sub>​ and should be configured as a sine wave with an amplitude greater than 6 volts, zero offset and a frequency of 100 Hz. The scope inputs are used to monitor various points around the circuit such as V<​sub>​IN</​sub>,​ V<​sub>​OUT</​sub>,​ the voltage across R<​sub>​S</​sub>​ and thus the current through R<​sub>​S</​sub>,​ and the gate of M<​sub>​1</​sub>​.+AWG1 is connected as V<​sub>​IN</​sub>​ and should be configured as a sine wave with an amplitude greater than 6 volts peak-to-peak, zero offset and a frequency of 100 Hz. The scope inputs are used to monitor various points around the circuit such as V<​sub>​IN</​sub>,​ V<​sub>​OUT</​sub>,​ the voltage across R<​sub>​S</​sub>​ and thus the current through R<​sub>​S</​sub>,​ and the gate of M<​sub>​1</​sub>​.
  
 {{ :​university:​courses:​electronics:​active_rectifiers_hardware_setup.png |}} {{ :​university:​courses:​electronics:​active_rectifiers_hardware_setup.png |}}
Line 82: Line 82:
 =====Questions:​===== =====Questions:​=====
  
-Change the peak amplitude of the AC input waveform. What is the minimum peak value of the AC input where the PMOS transistor is still actively rectifying the input, i.e. the V<​sub>​GS</​sub>​ is greater than the threshold voltage and the device is turned on? What determines this minimum voltage?+Change the peak-to-peak amplitude of the AC input waveform. What is the minimum peak value of the AC input where the PMOS transistor is still actively rectifying the input, i.e. the V<​sub>​GS</​sub>​ is greater than the threshold voltage and the device is turned on? What determines this minimum voltage?
  
 Try different frequencies for the AC input. How does the frequency effect the peak value and the width  of the current pulse in R<​sub>​S</​sub>?​ Try different frequencies for the AC input. How does the frequency effect the peak value and the width  of the current pulse in R<​sub>​S</​sub>?​
Line 94: Line 94:
 <WRAP round download>​ <WRAP round download>​
 **Resources:​** **Resources:​**
-  * Fritzing files: [[ https://​minhaskamal.github.io/​DownGit/#/​home?​url=https://​github.com/​analogdevicesinc/​education_tools/​tree/​master/​m2k/​fritzing/​active_rectifier_bb | active_rectifier_bb]] +  * Fritzing files: [[downgit>education_tools/​tree/​master/​m2k/​fritzing/​active_rectifier_bb | active_rectifier_bb]] 
-  * LTspice files: [[ https://​minhaskamal.github.io/​DownGit/#/​home?​url=https://​github.com/​analogdevicesinc/​education_tools/​tree/​master/​m2k/​ltspice/​active_rectifier_ltspice | active_rectifier_ltspice ]]+  * LTspice files: [[downgit>education_tools/​tree/​master/​m2k/​ltspice/​active_rectifier_ltspice | active_rectifier_ltspice ]]
 </​WRAP>​ </​WRAP>​
  
university/courses/electronics/electronics-lab-32.1551785677.txt.gz · Last modified: 05 Mar 2019 12:34 by Antoniu Miclaus