This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
university:courses:electronics:electronics-lab-32 [06 Feb 2014 19:41] – created Doug Mercer | university:courses:electronics:electronics-lab-32 [25 Jun 2020 22:07] (current) – external edit 127.0.0.1 | ||
---|---|---|---|
Line 16: | Line 16: | ||
=====Materials: | =====Materials: | ||
- | + | ADALM2000 Active Learning Module\\ | |
- | Analog Discovery Instrument\\ | + | |
Solder-less Breadboard\\ | Solder-less Breadboard\\ | ||
Jumper wires\\ | Jumper wires\\ | ||
Line 62: | Line 61: | ||
=====Hardware Setup:===== | =====Hardware Setup:===== | ||
- | AWG1 is connected as V< | + | AWG1 is connected as V< |
+ | |||
+ | {{ : | ||
+ | |||
+ | <WRAP centeralign> | ||
=====Procedure: | =====Procedure: | ||
Line 68: | Line 71: | ||
Start by using the large value 220 uF capacitor for C< | Start by using the large value 220 uF capacitor for C< | ||
- | Use the two scope inputs to monitor the input AC waveform at V< | + | Use the two scope inputs to monitor the input AC waveform at V< |
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
With scope channel 2 connected across shunt the 10Ω resistor R< | With scope channel 2 connected across shunt the 10Ω resistor R< | ||
Line 74: | Line 82: | ||
=====Questions: | =====Questions: | ||
- | Change the peak amplitude of the AC input waveform. What is the minimum peak value of the AC input where the PMOS transistor is still actively rectifying the input, i.e. the V< | + | Change the peak-to-peak amplitude of the AC input waveform. What is the minimum peak value of the AC input where the PMOS transistor is still actively rectifying the input, i.e. the V< |
Try different frequencies for the AC input. How does the frequency effect the peak value and the width of the current pulse in R< | Try different frequencies for the AC input. How does the frequency effect the peak value and the width of the current pulse in R< | ||
Line 83: | Line 91: | ||
There are other potential uses for a circuit that essentially allows current flow in only one direction with very low voltage drop across the switch. In battery chargers, where the input power source might be intermittent such as a solar panel or wind turbine generator, it is necessary to prevent the battery from discharging when the input power source is not generating a high enough voltage to charge the battery. Generally a simple Schottky diode is used for this purpose but as was pointed out in the background section this can lead to losses in efficiency. If an op amp with sufficiently low operating supply current is employed this can often be lower than the reverse leakage current in a large Schottky diode. | There are other potential uses for a circuit that essentially allows current flow in only one direction with very low voltage drop across the switch. In battery chargers, where the input power source might be intermittent such as a solar panel or wind turbine generator, it is necessary to prevent the battery from discharging when the input power source is not generating a high enough voltage to charge the battery. Generally a simple Schottky diode is used for this purpose but as was pointed out in the background section this can lead to losses in efficiency. If an op amp with sufficiently low operating supply current is employed this can often be lower than the reverse leakage current in a large Schottky diode. | ||
+ | |||
+ | <WRAP round download> | ||
+ | **Resources: | ||
+ | * Fritzing files: [[downgit> | ||
+ | * LTspice files: [[downgit> | ||
+ | </ | ||
**For Further Reading:** | **For Further Reading:** |