Next revision Both sides next revision
university:courses:electronics:electronics-lab-32 [24 Jul 2017 16:11]
Antoniu Miclaus change amplitude value to peak-peak
university:courses:electronics:electronics-lab-32 [10 Nov 2017 02:40]
Dann Kristofer Bautista added scope shot for vout and vin on both 220uF and 4.7uF
Line 62: Line 62:
  
 AWG1 is connected as V<​sub>​IN</​sub>​ and should be configured as a sine wave with an amplitude greater than 6 volts, zero offset and a frequency of 100 Hz. The scope inputs are used to monitor various points around the circuit such as V<​sub>​IN</​sub>,​ V<​sub>​OUT</​sub>,​ the voltage across R<​sub>​S</​sub>​ and thus the current through R<​sub>​S</​sub>,​ and the gate of M<​sub>​1</​sub>​. AWG1 is connected as V<​sub>​IN</​sub>​ and should be configured as a sine wave with an amplitude greater than 6 volts, zero offset and a frequency of 100 Hz. The scope inputs are used to monitor various points around the circuit such as V<​sub>​IN</​sub>,​ V<​sub>​OUT</​sub>,​ the voltage across R<​sub>​S</​sub>​ and thus the current through R<​sub>​S</​sub>,​ and the gate of M<​sub>​1</​sub>​.
 +
 +{{ :​university:​courses:​electronics:​active_rectifiers_hardware_setup.png |}}
 +
 +<WRAP centeralign>​ Figure 2 Active half wave rectifier with self-powered op amp Bread Board Circuit </​WRAP>​
  
 =====Procedure:​===== =====Procedure:​=====
Line 67: Line 71:
 Start by using the large value 220 uF capacitor for C<​sub>​1</​sub>​. The 220 uF and 4.7 uF capacitors are polarized so be sure to connect the positive and negative terminals to your circuit correctly. Start by using the large value 220 uF capacitor for C<​sub>​1</​sub>​. The 220 uF and 4.7 uF capacitors are polarized so be sure to connect the positive and negative terminals to your circuit correctly.
  
-Use the two scope inputs to monitor the input AC waveform at V<​sub>​IN</​sub>​ and the DC output wave form at V<​sub>​OUT</​sub>​. VOUT should be very close to the peak value of V<​sub>​IN</​sub>​. Now replace the large 220 uF capacitor with the much smaller 4.7 uF capacitor. Observe the change in the waveform seen at V<​sub>​OUT</​sub>​. When is V<​sub>​OUT</​sub>​ closest in value to V<​sub>​IN</​sub>​ and compare that interval of the AC input cycle with the voltage at the gate of transistor M<​sub>​1</​sub>​.+Use the two scope inputs to monitor the input AC waveform at V<​sub>​IN</​sub>​ and the DC output wave form at V<​sub>​OUT</​sub>​. VOUT should be very close to the peak value of V<​sub>​IN</​sub>​. Now replace the large 220 uF capacitor with the much smaller 4.7 uF capacitor. Observe the change in the waveform seen at V<​sub>​OUT</​sub>​. When is V<​sub>​OUT</​sub>​ closest in value to V<​sub>​IN</​sub>​ and compare that interval of the AC input cycle with the voltage at the gate of transistor M<​sub>​1</​sub>​. ​\\ 
 + 
 +{{ :​university:​courses:​electronics:​active_rectifiers_scopeshot_220uf.png |}} 
 +<WRAP centeralign>​ Figure 3 Vout and Vin at 220uF capacitor </​WRAP>​ 
 +{{ :​university:​courses:​electronics:​active_rectifiers_scopeshot_4.7uf.png |}} 
 +<WRAP centeralign>​ Figure 3 Vout and Vin at 4.7uF capacitor </​WRAP>​
  
 With scope channel 2 connected across shunt the 10Ω resistor R<​sub>​S</​sub>,​ use the Measure feature to obtain the peak and average value of the current. Compare the average value with the DC current in the 2.2 KΩ load resistor R<​sub>​L</​sub>​ you calculate based on the voltage you measure at V<​sub>​OUT</​sub>​. Repeat this measurement for both the 220 uF and 4.7 uF capacitor values. How do the peak and average values compare between these two capacitor values? ​ With scope channel 2 connected across shunt the 10Ω resistor R<​sub>​S</​sub>,​ use the Measure feature to obtain the peak and average value of the current. Compare the average value with the DC current in the 2.2 KΩ load resistor R<​sub>​L</​sub>​ you calculate based on the voltage you measure at V<​sub>​OUT</​sub>​. Repeat this measurement for both the 220 uF and 4.7 uF capacitor values. How do the peak and average values compare between these two capacitor values? ​
university/courses/electronics/electronics-lab-32.txt · Last modified: 25 Jun 2020 22:07 (external edit)