This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-30 [24 Jul 2017 16:13] – change amplitude value to peak-peak Antoniu Miclaus | university:courses:electronics:electronics-lab-30 [15 Dec 2017 03:37] – Added breadboard circuit and scopeshots for the lab sections Dann Kristofer Bautista | ||
---|---|---|---|
Line 75: | Line 75: | ||
used to monitor the inputs and outputs of the circuit as needed. The fixed +5 V power supply is to be | used to monitor the inputs and outputs of the circuit as needed. The fixed +5 V power supply is to be | ||
used to power your circuit. The fixed -5V supply should be disabled during this Lab. | used to power your circuit. The fixed -5V supply should be disabled during this Lab. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | <WRAP centeralign> | ||
=====Procedure: | =====Procedure: | ||
Line 85: | Line 89: | ||
First apply logic Low to A by opening the AWG control screen and setting AWG1 to 0 V DC. Apply logic low | First apply logic Low to A by opening the AWG control screen and setting AWG1 to 0 V DC. Apply logic low | ||
to the B input by setting AWG2 to 0 V DC. | to the B input by setting AWG2 to 0 V DC. | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
Observe the output C of the gate on scope Channel 1. A steady DC voltage should appear on the scope | Observe the output C of the gate on scope Channel 1. A steady DC voltage should appear on the scope | ||
Line 147: | Line 154: | ||
{{ : | {{ : | ||
- | + | <WRAP centeralign> | |
- | <WRAP centeralign> | + | |
=====Hardware Setup:===== | =====Hardware Setup:===== | ||
Configure both AWG channels as square waves with 5 V amplitudes and 2.5 V offsets ( 0 to 5 V swings). | Configure both AWG channels as square waves with 5 V amplitudes and 2.5 V offsets ( 0 to 5 V swings). | ||
- | Set both AWG1 and AWG2 to a frequency of 10 KHz. Also be sure to start with the phase of both AWG1 and | + | Set both AWG1 and AWG2 to a frequency of 1 KHz. Also be sure to start with the phase of both AWG1 and |
AWG2 set to 0°. Be sure to set the AWGs to run synchronously. | AWG2 set to 0°. Be sure to set the AWGs to run synchronously. | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
=====Procedure: | =====Procedure: | ||
Line 163: | Line 172: | ||
AWG 2 to the values listed in the table and record the DC voltage you observe at the output of the phase | AWG 2 to the values listed in the table and record the DC voltage you observe at the output of the phase | ||
detector. | detector. | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
^AWG1 Phase^AWG2 Phase^Output Voltage^ | ^AWG1 Phase^AWG2 Phase^Output Voltage^ |