Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
university:courses:electronics:electronics-lab-28 [05 Mar 2019 12:36]
amiclaus [Making a SPDT Analog Switch with the CD4007 transistor array]
university:courses:electronics:electronics-lab-28 [23 Aug 2019 14:03] (current)
amiclaus
Line 39: Line 39:
 ===== Hardware Setup: ===== ===== Hardware Setup: =====
  
-Configure the waveform generator for a 1 KHz triangle wave with 5V amplitude and 2.5V offset. Both scope channels should be set to 1V/Div. Configure the scope in XY mode with channel 1 on the horizontal axis and channel 2 on the vertical axis.+Configure the waveform generator for a 1 KHz triangle wave with 5V amplitude ​peak-to-peak ​and 2.5V offset. Both scope channels should be set to 1V/Div. Configure the scope in XY mode with channel 1 on the horizontal axis and channel 2 on the vertical axis.
 {{ :​university:​courses:​electronics:​a28_f3bb.JPG?​ |}} {{ :​university:​courses:​electronics:​a28_f3bb.JPG?​ |}}
  
Line 80: Line 80:
 ===== Hardware Setup: ===== ===== Hardware Setup: =====
  
-Now configure the waveform generator for a 500 KHz square wave with 5V amplitude and 2.5V offset. Be sure to reconnect scope channel 2 to measure the output voltage waveform. Both scope channels should be set to 1V/Div. Adjust the horizontal scale so that you can view both the rising and falling edges of the input and output waveforms similar to what is shown in figures 7 and 8.+Now configure the waveform generator for a 500 KHz square wave with 5V amplitude ​peak-to-peak ​and 2.5V offset. Be sure to reconnect scope channel 2 to measure the output voltage waveform. Both scope channels should be set to 1V/Div. Adjust the horizontal scale so that you can view both the rising and falling edges of the input and output waveforms similar to what is shown in figures 7 and 8.
 {{ :​university:​courses:​electronics:​a28_nf9a.PNG?​ |}} {{ :​university:​courses:​electronics:​a28_nf9a.PNG?​ |}}
  
Line 112: Line 112:
 ===== Hardware Setup: ===== ===== Hardware Setup: =====
  
-Configure the waveform generator for a 1 KHz triangle wave with 5V amplitude and 2.5V offset. Both scope channels should be set to 1V/Div. Configure the scope in XY mode with channel 1 on the horizontal axis and channel 2 on the vertical axis.+Configure the waveform generator for a 1 KHz triangle wave with 5V amplitude ​peak-to-peak ​and 2.5V offset. Both scope channels should be set to 1V/Div. Configure the scope in XY mode with channel 1 on the horizontal axis and channel 2 on the vertical axis.
 {{ :​university:​courses:​electronics:​a28_f12a.png?​ |}} {{ :​university:​courses:​electronics:​a28_f12a.png?​ |}}
  
university/courses/electronics/electronics-lab-28.txt · Last modified: 23 Aug 2019 14:03 by amiclaus