This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:courses:electronics:electronics-lab-28 [31 Jan 2019 08:19] – Trecia Agoylo | university:courses:electronics:electronics-lab-28 [14 Jun 2022 14:11] (current) – [Making inverters with the CD4007 transistor array] Doug Mercer | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== Build CMOS Logic Functions Using CD4007 Array ====== | + | ====== Build CMOS Logic Functions Using CD4007 Array - ADALM2000====== |
===== Objective: ===== | ===== Objective: ===== | ||
Line 9: | Line 9: | ||
Below in figure 1 is the schematic and pinout for the CD4007: | Below in figure 1 is the schematic and pinout for the CD4007: | ||
- | {{ : | + | {{ : |
<WRAP centeralign> | <WRAP centeralign> | ||
Line 39: | Line 39: | ||
===== Hardware Setup: ===== | ===== Hardware Setup: ===== | ||
- | Configure the waveform generator for a 1 KHz triangle wave with 5V amplitude and 2.5V offset. Both scope channels should be set to 1V/Div. Configure the scope in XY mode with channel 1 on the horizontal axis and channel 2 on the vertical axis. | + | Configure the waveform generator for a 100 Hz triangle wave with 5V amplitude |
{{ : | {{ : | ||
Line 80: | Line 80: | ||
===== Hardware Setup: ===== | ===== Hardware Setup: ===== | ||
- | Now configure the waveform generator for a 500 KHz square wave with 5V amplitude and 2.5V offset. Be sure to reconnect scope channel 2 to measure the output voltage waveform. Both scope channels should be set to 1V/Div. Adjust the horizontal scale so that you can view both the rising and falling edges of the input and output waveforms similar to what is shown in figures 7 and 8. | + | Now configure the waveform generator for a 500 KHz square wave with 5V amplitude |
- | {{ : | + | {{ : |
<WRAP centeralign> | <WRAP centeralign> | ||
Line 112: | Line 112: | ||
===== Hardware Setup: ===== | ===== Hardware Setup: ===== | ||
- | Configure the waveform generator for a 1 KHz triangle wave with 5V amplitude and 2.5V offset. Both scope channels should be set to 1V/Div. Configure the scope in XY mode with channel 1 on the horizontal axis and channel 2 on the vertical axis. | + | Configure the waveform generator for a 1 KHz triangle wave with 5V amplitude |
{{ : | {{ : | ||
Line 214: | Line 214: | ||
The on resistance, R< | The on resistance, R< | ||
+ | <WRAP round download> | ||
+ | **Resources: | ||
+ | * Fritzing files: [[downgit> | ||
+ | * LTspice files: [[downgit> | ||
+ | </ | ||
===== For Further reading: ===== | ===== For Further reading: ===== | ||
- | 4000 Series Logic and Analog Circuitry: http:// | + | {{ : |
CMOS Logic: http:// | CMOS Logic: http:// | ||
Noise Margin: http:// | Noise Margin: http:// |