This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-28 [05 Mar 2019 12:36] – [Making a SPDT Analog Switch with the CD4007 transistor array] Antoniu Miclaus | university:courses:electronics:electronics-lab-28 [23 Aug 2019 14:03] – Antoniu Miclaus | ||
---|---|---|---|
Line 39: | Line 39: | ||
===== Hardware Setup: ===== | ===== Hardware Setup: ===== | ||
- | Configure the waveform generator for a 1 KHz triangle wave with 5V amplitude and 2.5V offset. Both scope channels should be set to 1V/Div. Configure the scope in XY mode with channel 1 on the horizontal axis and channel 2 on the vertical axis. | + | Configure the waveform generator for a 1 KHz triangle wave with 5V amplitude |
{{ : | {{ : | ||
Line 80: | Line 80: | ||
===== Hardware Setup: ===== | ===== Hardware Setup: ===== | ||
- | Now configure the waveform generator for a 500 KHz square wave with 5V amplitude and 2.5V offset. Be sure to reconnect scope channel 2 to measure the output voltage waveform. Both scope channels should be set to 1V/Div. Adjust the horizontal scale so that you can view both the rising and falling edges of the input and output waveforms similar to what is shown in figures 7 and 8. | + | Now configure the waveform generator for a 500 KHz square wave with 5V amplitude |
{{ : | {{ : | ||
Line 112: | Line 112: | ||
===== Hardware Setup: ===== | ===== Hardware Setup: ===== | ||
- | Configure the waveform generator for a 1 KHz triangle wave with 5V amplitude and 2.5V offset. Both scope channels should be set to 1V/Div. Configure the scope in XY mode with channel 1 on the horizontal axis and channel 2 on the vertical axis. | + | Configure the waveform generator for a 1 KHz triangle wave with 5V amplitude |
{{ : | {{ : | ||