Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
university:courses:electronics:electronics-lab-27 [08 Jul 2022 15:35] – [Materials:] Doug Merceruniversity:courses:electronics:electronics-lab-27 [08 Jul 2022 15:36] (current) – [Background:] Doug Mercer
Line 31: Line 31:
 <WRAP centeralign> Figure 4 Output Stage </WRAP> <WRAP centeralign> Figure 4 Output Stage </WRAP>
  
-The diode, D<sub>1</sub>, serves to increase the effective turn on voltage of Q<sub>4</sub> which allows it to be turned off before Q<sub>3</sub>turns fully on. This helps prevent potentially large surge currents from flowing in the output stage during transitions between logic states. Resistor R<sub>4</sub> also serves to limit the current that is allowed to flow in the output stage. The disadvantage is that the logic high voltage is reduced by an amount of the diode drop as shown in figure 6.+The diode, D<sub>1</sub>, serves to increase the effective turn on voltage of Q<sub>4</sub> which allows it to be turned off before Q<sub>3</sub>turns fully on. This helps prevent potentially large surge currents from flowing in the output stage during transitions between logic states. Resistor R<sub>4</sub> also serves to limit the current that is allowed to flow in the output stage. The disadvantage is that the logic high voltage is reduced by an amount of the diode drop as shown in figure 7.
 ===== Materials: ===== ===== Materials: =====
 ADALM2000 Active Learning Module\\ ADALM2000 Active Learning Module\\
university/courses/electronics/electronics-lab-27.txt · Last modified: 08 Jul 2022 15:36 by Doug Mercer