This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-24 [24 Jul 2017 16:12] – change amplitude value to peak-peak Antoniu Miclaus | university:courses:electronics:electronics-lab-24 [24 Nov 2017 08:12] – Uploaded Monostable and Bistable scopeshot Dann Kristofer Bautista | ||
---|---|---|---|
Line 34: | Line 34: | ||
Turn on the Vp power supply only after you have completely built and checked the circuit. The red and green LEDs should alternately blink on and off at about a 1 second interval. You can also use the scope channels to monitor the output waveforms (Q and Qbar). | Turn on the Vp power supply only after you have completely built and checked the circuit. The red and green LEDs should alternately blink on and off at about a 1 second interval. You can also use the scope channels to monitor the output waveforms (Q and Qbar). | ||
+ | \\ \\ | ||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | \\ | ||
The frequency of oscillation is very slow due to the large values of capacitors C< | The frequency of oscillation is very slow due to the large values of capacitors C< | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
===== Questions: ===== | ===== Questions: ===== | ||
Line 71: | Line 79: | ||
{{ : | {{ : | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
===== Procedure: ===== | ===== Procedure: ===== | ||
Turn on the Vp power supply only after you have completely built and checked the circuit. The red LED should be lit and the green LED should be dark. With a length of wire, momentarily touch the trigger input (end of R< | Turn on the Vp power supply only after you have completely built and checked the circuit. The red LED should be lit and the green LED should be dark. With a length of wire, momentarily touch the trigger input (end of R< | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | |||
===== Questions: ===== | ===== Questions: ===== | ||
Line 81: | Line 96: | ||
Add questions here: | Add questions here: | ||
- | ====== The BIstable | + | ====== The Bistable |
===== Objectives: ===== | ===== Objectives: ===== | ||
Line 105: | Line 120: | ||
{{ : | {{ : | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
+ | |||
+ | {{ : | ||
+ | |||
+ | <WRAP centeralign> | ||
===== Procedure: ===== | ===== Procedure: ===== | ||
Turn on the Vp power supply only after you have completely built and checked the circuit. Either the red LED should be lit with the green LED dark or the green LED should be lit with the red LED dark. With a length of wire, momentarily touch the either the SET or RESET input (end of R< | Turn on the Vp power supply only after you have completely built and checked the circuit. Either the red LED should be lit with the green LED dark or the green LED should be lit with the red LED dark. With a length of wire, momentarily touch the either the SET or RESET input (end of R< | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
Connect the SET and RESET inputs to two of the digital I/O pins on the ADALM2000 connector. Configure | Connect the SET and RESET inputs to two of the digital I/O pins on the ADALM2000 connector. Configure | ||
the pins as push-pull outputs. Used the static digital I/O screen to control the digital pins. | the pins as push-pull outputs. Used the static digital I/O screen to control the digital pins. | ||
+ | |||
+ | |||
===== Questions: ===== | ===== Questions: ===== | ||
Line 169: | Line 196: | ||
{{ : | {{ : | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
====Hardware setup:==== | ====Hardware setup:==== | ||
Line 179: | Line 206: | ||
swing ). Set the frequency of AWG1 to 10 KHz and set the frequency of AWG2 to 5 KHz. Set the phase of | swing ). Set the frequency of AWG1 to 10 KHz and set the frequency of AWG2 to 5 KHz. Set the phase of | ||
AWG2 to 45 degrees. Be sure to configure the two AWG outputs to operate synchronously. | AWG2 to 45 degrees. Be sure to configure the two AWG outputs to operate synchronously. | ||
+ | \\ | ||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
====Procedure: | ====Procedure: | ||
Line 188: | Line 218: | ||
should see a similar square wave signal but ahead in time with respect to the Q output. In other words | should see a similar square wave signal but ahead in time with respect to the Q output. In other words | ||
the Q output is delayed until the falling edge of the Clock signal. | the Q output is delayed until the falling edge of the Clock signal. | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
====Questions: | ====Questions: | ||
Line 252: | Line 287: | ||
{{ : | {{ : | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
====Hardware setup:==== | ====Hardware setup:==== | ||
The AWG1 output and scope channel 1 input should both be connected to the input marked Clock in figure | The AWG1 output and scope channel 1 input should both be connected to the input marked Clock in figure | ||
- | 5. The second input scope channel 2 should be connected to the Q output of the flip-flop in figure 5. | + | 13. The second input scope channel 2 should be connected to the Q output of the flip-flop in figure 5. |
The AWG1 should be configured as a square wave with a 5 V amplitude and 2.5 V offset ( 0 - 5V swing ). | The AWG1 should be configured as a square wave with a 5 V amplitude and 2.5 V offset ( 0 - 5V swing ). | ||
Set the frequency to 10 KHz. | Set the frequency to 10 KHz. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | <WRAP centeralign> | ||
====Procedure: | ====Procedure: | ||
Line 267: | Line 306: | ||
signal. Move the channel 2 scope input to the QB output. You should see a similar square wave signal but | signal. Move the channel 2 scope input to the QB output. You should see a similar square wave signal but | ||
inverted with respect to the Q output. | inverted with respect to the Q output. | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
====Questions: | ====Questions: |