Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revisionBoth sides next revision
university:courses:electronics:electronics-lab-24 [12 Jul 2019 14:16] Pop Andreeauniversity:courses:electronics:electronics-lab-24 [23 Aug 2019 14:02] Antoniu Miclaus
Line 203: Line 203:
 connected to the D input. The first scope channel 1 input should also be connected to Clock input. The  connected to the D input. The first scope channel 1 input should also be connected to Clock input. The 
 second input scope channel 2 should be connected to the Q output of the flip-flop in figure 4. Both the  second input scope channel 2 should be connected to the Q output of the flip-flop in figure 4. Both the 
-AWG1 and AWG2 should be configured as a square wave with a 5 V amplitude and 2.5 V offset ( 0 - 5V +AWG1 and AWG2 should be configured as a square wave with a 5 V amplitude peak-to-peak and 2.5 V offset ( 0 - 5V 
 swing ). Set the frequency of AWG1 to 10 KHz and set the frequency of AWG2 to 5 KHz. Set the phase of  swing ). Set the frequency of AWG1 to 10 KHz and set the frequency of AWG2 to 5 KHz. Set the phase of 
 AWG2 to 45 degrees. Be sure to configure the two AWG outputs to operate synchronously.  AWG2 to 45 degrees. Be sure to configure the two AWG outputs to operate synchronously. 
Line 293: Line 293:
 The AWG1 output and scope channel 1 input should both be connected to the input marked Clock in figure  The AWG1 output and scope channel 1 input should both be connected to the input marked Clock in figure 
 13. The second input scope channel 2 should be connected to the Q output of the flip-flop in figure 5.  13. The second input scope channel 2 should be connected to the Q output of the flip-flop in figure 5. 
-The AWG1 should be configured as a square wave with a 5 V amplitude and 2.5 V offset ( 0 - 5V swing ). +The AWG1 should be configured as a square wave with a 5 V amplitude peak-to-peak and 2.5 V offset ( 0 - 5V swing ). 
 Set the frequency to 10 KHz. Set the frequency to 10 KHz.
  
university/courses/electronics/electronics-lab-24.txt · Last modified: 03 Nov 2021 20:43 by Doug Mercer