Wiki

This version is outdated by a newer approved version.DiffThis version (25 Jun 2020 22:07) is a draft.
Approvals: 0/1
The Previously approved version (23 Jan 2020 21:54) is available.Diff

This is an old revision of the document!


Activity: The CMOS Analog Switch

Objective:

The objective of this exercise is to explore the use of complementary MOS transistors as an analog voltage switch.

Concept:

The ideal analog switch has no on-resistance, infinite off-impedance and zero time delay, and can handle large signal and common-mode voltages. Real analog switches made with MOS transistors meet none of these criteria, but if we understand the limitations of analog switches, most of these limitations can be overcome. The on-resistance is one of these limitations and this lab activity will attempt to characterize this switch specification.

Materials:

ADALM2000 Active Learning Module
Solder-less breadboard
Jumper wires
1 - CD4007 CMOS transistor array
2 - NPN transistors (2N3904 or equivalent)
1 - 4.7 KΩ resistor

CD4007 CMOS transistor array pinout

NMOS Directions:

Construct the test circuit shown in figure 1. The green boxes indicate connections to the connector on ADALM2000. NMOS and PMOS devices M1 and M2 are contained in the CD4007 package. All un-used pins can be left floating. To measure the resistance (Ron) of the MOS transistors we first need to force a known current through the resistance and then measure the voltage across the resistance. The two NPN devices Q1 and Q2 along with resistor R1 form a current source with an output current of approximately 1 mA. The exact magnitude of this current is not important in that we are mainly interested in the change in the Ron of the MOS devices as the voltage at their source/drain varies over the range of between the plus and minus power supplies.

In this first test only NMOS device M1 is turned on and PMOS device M2 is turned off.

Figure 1 NMOS Ron test circuit

Hardware Setup:

Figure 2 NMOS Ron test circuit Breadboard Connections

Procedure:

Configure waveform generator 1 as a 100 Hz triangle wave with an amplitude of 9 volts peak-to-peak and an offset of +500 mV. This will swing the voltage on the NMOS switch transistor from +5 volts to -4 volts. We can not swing the voltage all the way to -5 volts because of the NPN current source Q2. Be sure to turn on the external user power supplies (Vp and Vn) before running the waveform generator. Configure the scope screen in XY mode with C1 on the X axis, and C2 (the voltage across the switch) on the Y axis. Use the math function to calculate the resistance (C2 / 1mA). Note: You can get a more precise estimate of the current source by measuring the voltage across R1 and its actual resistance.

Figure 3 NMOS Ron X-Y trace

Questions:

At what voltage does the NMOS devices turn off?

What happens to the source to drain voltage as the NMOS transistor turns off?

How does this affect the display on the scope screen?

PMOS Directions:

Now modify your circuit to look like figure 2 by connecting the gates of both M1 and M2 to the negative power supply Vn. In this second test only PMOS device M2 is turned on and NMOS device M1 is turned off.

Figure 4 PMOS Ron test circuit

Hardware Setup:

Figure 5 PMOS Ron test circuit Breadboard Connections

Procedure:

Repeat the sweep of the voltage from waveform generator W1 and plot the on-resistance of just the PMOS transistor.

Figure 6 PMOS Ron X-Y trace

Questions:

At what voltage does the PMOS devices turn off?

What happens to the source to drain voltage as the PMOS transistor turns off?

How does this affect the display on the scope screen?

CMOS Directions:

Now modify your circuit to look like figure 3 by connecting the gate of M1 to the positive power supply Vp and the gate of M2 to the negative power supply Vn. In this last test both NMOS device M1 and PMOS device M2 is turned on.

Figure 7 CMOS Ron test circuit

Hardware Setup:

Figure 8 CMOS Ron test circuit Breadboard Connections

Procedure:

Repeat the sweep of the voltage and plot the on resistance of the combined NMOS and PMOS transistors.

Figure 9 CMOS Ron X-Y trace

Questions:

Do either the NMOS or PMOS transistors ever turn off?

Are both the NMOS and PMOS ever off at the same time?

If an NMOS switch is used to connect two signal nodes that can have analog voltages that vary from 0 to 1V, what must be the value of the bulk and gate voltages for the switch to work properly?

What are the conditions for a PMOS switch?

For Further Study:

Extra Challenge Activity:

Try measuring the Ron vs input voltage for other CMOS analog switches such as the CD4016, CD4066 quad switches or the CD4051, CD4052, and CD4053 analog multiplexers or the ADG419 SPDT analog switch or ADG333 quad SPDT switch. Compare your results to the Ron specified in the manufacturer product datasheets.

Resources:

Return to Lab Activity Table of Contents

university/courses/electronics/electronics-lab-18.1593115655.txt.gz · Last modified: 25 Jun 2020 22:07 by