This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-18 [25 Jan 2019 13:43] – add ltspice files Antoniu Miclaus | university:courses:electronics:electronics-lab-18 [23 Aug 2019 13:51] – Antoniu Miclaus | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== Activity | + | ====== Activity: The CMOS Analog Switch====== |
===== Objective: ===== | ===== Objective: ===== | ||
Line 38: | Line 38: | ||
===== Procedure: ===== | ===== Procedure: ===== | ||
- | Configure waveform generator 1 as a 100 Hz triangle wave with an amplitude of 9 volts and an offset of +500 mV. This will swing the voltage on the NMOS switch transistor from +5 volts to -4 volts. We can not swing the voltage all the way to -5 volts because of the NPN current source Q< | + | Configure waveform generator 1 as a 100 Hz triangle wave with an amplitude of 9 volts peak-to-peak |
{{ : | {{ : | ||
Line 119: | Line 119: | ||
Try measuring the Ron vs input voltage for other CMOS analog switches such as the CD4016, CD4066 quad switches or the CD4051, CD4052, and CD4053 analog multiplexers or the ADG419 SPDT analog switch or ADG333 quad SPDT switch. Compare your results to the Ron specified in the manufacturer product datasheets. | Try measuring the Ron vs input voltage for other CMOS analog switches such as the CD4016, CD4066 quad switches or the CD4051, CD4052, and CD4053 analog multiplexers or the ADG419 SPDT analog switch or ADG333 quad SPDT switch. Compare your results to the Ron specified in the manufacturer product datasheets. | ||
+ | <WRAP round download> | ||
**Resources: | **Resources: | ||
* Fritzing files: [[ https:// | * Fritzing files: [[ https:// | ||
* LTspice files: [[ https:// | * LTspice files: [[ https:// | ||
+ | </ | ||
**Return to Lab Activity [[university: | **Return to Lab Activity [[university: | ||