This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:courses:electronics:electronics-lab-16 [24 Apr 2017 08:46] – rename Antoniu Miclaus | university:courses:electronics:electronics-lab-16 [14 Jun 2022 14:06] (current) – [Appendix:] Doug Mercer | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== Activity | + | ====== Activity: DC-DC Converters II - ADALM2000====== |
===== Objective: ===== | ===== Objective: ===== | ||
Line 84: | Line 84: | ||
===== Questions: ===== | ===== Questions: ===== | ||
What other types of oscillator circuits might be used to generate the 100 KHz square wave? | What other types of oscillator circuits might be used to generate the 100 KHz square wave? | ||
- | |||
- | ==== For further reading: ==== | ||
- | |||
- | [[http:// | ||
- | |||
- | [[http:// | ||
- | |||
- | [[http:// | ||
- | |||
- | **Return to Lab Activity [[university: | ||
- | |||
====== Appendix: ====== | ====== Appendix: ====== | ||
Line 106: | Line 95: | ||
CD4007 Pinout: | CD4007 Pinout: | ||
- | {{ : | + | {{ : |
<WRAP centeralign> | <WRAP centeralign> | ||
Line 121: | Line 110: | ||
Two of these inverters can be used to construct the inverters needed in figure 3. | Two of these inverters can be used to construct the inverters needed in figure 3. | ||
+ | |||
+ | ==== For further reading: ==== | ||
+ | [[adi> | ||
+ | [[wp> | ||
+ | [[wp> | ||
+ | [[adi> | ||
+ | |||
+ | **Return to Lab Activity [[university: | ||
+ | |||