This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-16 [23 Mar 2017 16:41] – [Materials:] Doug Mercer | university:courses:electronics:electronics-lab-16 [12 Jul 2019 14:08] – Pop Andreea | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== Activity | + | ====== Activity: DC-DC Converters II ====== |
===== Objective: ===== | ===== Objective: ===== | ||
Line 47: | Line 47: | ||
===== Procedure: ===== | ===== Procedure: ===== | ||
- | Be sure to start up the digital pulse source output on the Analog Discovery | + | Be sure to start up the digital pulse source output on the ADALM2000 |
===== Questions: ===== | ===== Questions: ===== | ||
Line 76: | Line 76: | ||
===== Circuit Additions: ===== | ===== Circuit Additions: ===== | ||
- | What sort of circuit could you make to generate the 100 KHz square wave other than using the digital pulse source output on the Analog Discovery | + | What sort of circuit could you make to generate the 100 KHz square wave other than using the digital pulse source output on the ADALM2000 |
{{ : | {{ : | ||
Line 84: | Line 84: | ||
===== Questions: ===== | ===== Questions: ===== | ||
What other types of oscillator circuits might be used to generate the 100 KHz square wave? | What other types of oscillator circuits might be used to generate the 100 KHz square wave? | ||
- | |||
- | ==== For further reading: ==== | ||
- | |||
- | [[http:// | ||
- | |||
- | [[http:// | ||
- | |||
- | [[http:// | ||
- | |||
- | **Return to Lab Activity [[university: | ||
- | |||
====== Appendix: ====== | ====== Appendix: ====== | ||
Line 121: | Line 110: | ||
Two of these inverters can be used to construct the inverters needed in figure 3. | Two of these inverters can be used to construct the inverters needed in figure 3. | ||
+ | |||
+ | ==== For further reading: ==== | ||
+ | |||
+ | [[http:// | ||
+ | |||
+ | [[http:// | ||
+ | |||
+ | [[http:// | ||
+ | |||
+ | **Return to Lab Activity [[university: | ||
+ | |||