This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-14 [20 Sep 2019 16:07] – [Unipolar output operation] Pop Andreea | university:courses:electronics:electronics-lab-14 [20 Sep 2019 16:12] – [Unipolar output operation] Pop Andreea | ||
---|---|---|---|
Line 73: | Line 73: | ||
the loaded value can be transferred to the DAC register by strobing the LDAC pin. | the loaded value can be transferred to the DAC register by strobing the LDAC pin. | ||
===== Unipolar output operation===== | ===== Unipolar output operation===== | ||
- | This mode of operation is the basic mode for AD5626. | + | This mode of operation is the basic mode for AD5626. |
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign > Figure 7. Unipolar code table of AD5626</ | ||
===Hardware setup=== | ===Hardware setup=== | ||
- | Connect the pins of AD5626 as shown in figure | + | Connect the pins of AD5626 as shown in figure |
{{ : | {{ : | ||
- | <WRAP centeralign > Figure | + | <WRAP centeralign > Figure |
- | {{ : | + | {{ : |
- | <WRAP centeralign > Figure | + | <WRAP centeralign > Figure |
Line 93: | Line 96: | ||
The signals of the SPI group channel should resemble the timing diagram of the AD5626 digital to analog converter. | The signals of the SPI group channel should resemble the timing diagram of the AD5626 digital to analog converter. | ||
- | {{ : | + | {{ : |
- | <WRAP centeralign > Figure | + | <WRAP centeralign > Figure |
Now you should configure /LDAC and /CLR signals. | Now you should configure /LDAC and /CLR signals. | ||
Line 108: | Line 111: | ||
The last step is to open oscilloscope and connect channel 1 to the output of AD5626. Enable channel 1 measurements and enter a value in the " | The last step is to open oscilloscope and connect channel 1 to the output of AD5626. Enable channel 1 measurements and enter a value in the " | ||
- | In figure | + | In figure |
{{ : | {{ : | ||
- | <WRAP centeralign > Figure | + | <WRAP centeralign > Figure |
=====Questions: | =====Questions: |