Next revision Both sides next revision
university:courses:electronics:electronics-lab-14 [20 Sep 2019 16:06]
Pop Andreea AD5626
university:courses:electronics:electronics-lab-14 [20 Sep 2019 16:12]
Pop Andreea [Unipolar output operation]
Line 73: Line 73:
 the loaded value can be transferred to the DAC register by strobing the LDAC pin. the loaded value can be transferred to the DAC register by strobing the LDAC pin.
 ===== Unipolar output operation===== ===== Unipolar output operation=====
-This mode of operation is the basic mode for AD5626.+This mode of operation is the basic mode for AD5626. ​You can verify the god functionality AD5626 according to the unipolar code table of the digital to analog convertor. 
 + 
 +{{ :​university:​courses:​electronics:​unipolar_code_table.png?​700 |}} 
 +<WRAP centeralign > Figure 7.  Unipolar code table of AD5626</​WRAP>​
 ===Hardware setup=== ===Hardware setup===
-Connect the pins of AD5626 as shown in figure ​7.+Connect the pins of AD5626 as shown in figure ​8.
 {{ :​university:​courses:​electronics:​connections_ad5626.png?​600 |}} {{ :​university:​courses:​electronics:​connections_ad5626.png?​600 |}}
-<WRAP centeralign > Figure ​7. Connections for Unipolar operation AD5626</​WRAP>​+<WRAP centeralign > Figure ​8. Connections for Unipolar operation AD5626</​WRAP>​
  
-{{ :​university:​courses:​electronics:​ad5626_bb_bb.png?​600 |}} +{{ :​university:​courses:​electronics:​ad5626_bb_bb.png?​900 |}} 
-<WRAP centeralign > Figure ​8. AD5626 breadboard connections</​WRAP>​+<WRAP centeralign > Figure ​9. AD5626 breadboard connections</​WRAP>​
  
  
Line 93: Line 96:
 The signals of the SPI group channel should resemble the timing diagram of the AD5626 digital to analog converter. The signals of the SPI group channel should resemble the timing diagram of the AD5626 digital to analog converter.
  
-{{ :​university:​courses:​electronics:​timing_diagram.png?​700 |}}  +{{ :​university:​courses:​electronics:​timing_diagram.png?​900 |}}  
-<WRAP centeralign > Figure ​9. AD5626 SPI timing diagram</​WRAP>​+<WRAP centeralign > Figure ​10. AD5626 SPI timing diagram</​WRAP>​
  
 Now you should configure /LDAC and /CLR signals. Now you should configure /LDAC and /CLR signals.
Line 105: Line 108:
 {{ :​university:​courses:​electronics:​07ff.png?​900 |}} {{ :​university:​courses:​electronics:​07ff.png?​900 |}}
  
-<WRAP centeralign > Figure ​10. Pattern generator signals setup</​WRAP>​+<WRAP centeralign > Figure ​11. Pattern generator signals setup</​WRAP>​
  
 The last step is to open oscilloscope and connect channel 1 to the output of AD5626. Enable channel 1 measurements and enter a value in the "​Data"​ area of SPI. The last step is to open oscilloscope and connect channel 1 to the output of AD5626. Enable channel 1 measurements and enter a value in the "​Data"​ area of SPI.
-In figure ​11 you can see the output voltage if the data sent through SPI is 7FF.+In figure ​12 you can see the output voltage if the data sent through SPI is 7FF.
  
 {{ :​university:​courses:​electronics:​vout_ad5626.png?​900 |}} {{ :​university:​courses:​electronics:​vout_ad5626.png?​900 |}}
-<WRAP centeralign > Figure ​10. AD5626 output voltage for 7FF input.</​WRAP>​+<WRAP centeralign > Figure ​12. AD5626 output voltage for 7FF input.</​WRAP>​
  
 =====Questions:​===== =====Questions:​=====
university/courses/electronics/electronics-lab-14.txt · Last modified: 25 Jun 2020 22:07 (external edit)