This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-13a [25 Oct 2017 05:20] – Trecia Agoylo | university:courses:electronics:electronics-lab-13a [25 Jun 2020 22:07] – external edit | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== Activity | + | ====== Activity: Amplifier Output Stages ====== |
===== Objective: ===== | ===== Objective: ===== | ||
Line 30: | Line 30: | ||
Channel one of the scope should be connected to display the output of the first generator and both scope channels 1 and 2 should be set to display 1V per division. The breadboard connections are shown in figure 2. | Channel one of the scope should be connected to display the output of the first generator and both scope channels 1 and 2 should be set to display 1V per division. The breadboard connections are shown in figure 2. | ||
- | {{ : | + | {{ : |
<WRAP centeralign> | <WRAP centeralign> | ||
Line 36: | Line 36: | ||
===== Procedure: ===== | ===== Procedure: ===== | ||
- | The waveform generator, W1, should be configured for a 1 KHz sine wave with 6.0 volt amplitude peak amplitude | + | The waveform generator, W1, should be configured for a 1 KHz sine wave with 6.0 volt amplitude peak-to-peak |
{{ : | {{ : | ||
<WRAP centeralign> | <WRAP centeralign> | ||
- | Next, apply power and adjust the waveform generator so that W1 is a 100 Hz triangle wave with 0V offset and 3.0 V amplitude | + | Next, apply power and adjust the waveform generator so that W1 is a 100 Hz triangle wave with 0V offset and 3.0 V amplitude |
{{ : | {{ : | ||
Line 54: | Line 54: | ||
• Starting with the amplitude = 0 V, gradually increase it until you just begin to see a signal on scope channel 2 appear at the output. For what range of amplitude values of W1 can we say that both BJT's are essentially off? Confirm this by observing the voltages of the current-sensing resistances R< | • Starting with the amplitude = 0 V, gradually increase it until you just begin to see a signal on scope channel 2 appear at the output. For what range of amplitude values of W1 can we say that both BJT's are essentially off? Confirm this by observing the voltages of the current-sensing resistances R< | ||
- | • Raise W1 to 6.0V amplitude value, and record the amplitude of the output waveform as well as the collector currents of the BJTs, which can be found via Ohm's law from the voltages across R< | + | • Raise W1 to 6.0V amplitude |
- | • Repeat, but with W1 raised a 10.0V amplitude value; and comment. | + | • Repeat, but with W1 raised a 10.0V amplitude |
Simulate the circuit of figure 1 using QUCS, compare with your lab findings, and justify any differences. | Simulate the circuit of figure 1 using QUCS, compare with your lab findings, and justify any differences. | ||
Line 74: | Line 74: | ||
===== Hardware Setup: ===== | ===== Hardware Setup: ===== | ||
- | Channel one of the scope should be connected to display the output of the first generator and both scope channels 1 and 2 should be set to display 1V per division. The breadboard connections are shown in figure | + | Channel one of the scope should be connected to display the output of the first generator and both scope channels 1 and 2 should be set to display 1V per division. The breadboard connections are shown in figure |
- | {{ : | + | {{ : |
<WRAP centeralign> | <WRAP centeralign> | ||
===== Procedure: ===== | ===== Procedure: ===== | ||
- | The waveform generator, W1, should be configured for a 1 KHz sine wave with 6.0 volt amplitude peak amplitude | + | The waveform generator, W1, should be configured for a 1 KHz sine wave with 6.0 volt amplitude peak-to-peak |
{{ : | {{ : | ||
Line 106: | Line 106: | ||
===== Hardware Setup: ===== | ===== Hardware Setup: ===== | ||
- | Channel one of the scope should be connected to display the output of the first generator and both scope channels 1 and 2 should be set to display 1V per division. The breadboard connections are shown in figure | + | Channel one of the scope should be connected to display the output of the first generator and both scope channels 1 and 2 should be set to display 1V per division. The breadboard connections are shown in figure |
- | {{ : | + | {{ : |
<WRAP centeralign> | <WRAP centeralign> | ||
===== Procedure: ===== | ===== Procedure: ===== | ||
- | The waveform generator, W1, should be configured for a 1 KHz sine wave with 6.0 volt amplitude peak amplitude | + | The waveform generator, W1, should be configured for a 1 KHz sine wave with 6.0 volt amplitude peak-to-peak |
{{ : | {{ : | ||
<WRAP centeralign> | <WRAP centeralign> | ||
+ | |||
+ | ** Lab Resources: | ||
+ | * LTSpice files: [[downgit> | ||
Line 126: | Line 129: | ||
Using your scope input, measure Vout as well as the voltage across R< | Using your scope input, measure Vout as well as the voltage across R< | ||
- | Measure the input impedance by inserting a 10K? resistor in series with the signal generator (between W1 and the bases of Q< | + | Measure the input impedance by inserting a 10KΩ resistor in series with the signal generator (between W1 and the bases of Q< |
- | Simulate the circuit of figure 3 using QUCS, compare with your lab findings, and justify any differences. | + | Simulate the circuit of figure 3 using LTSpice or ADIsimPE, compare with your lab findings, and justify any differences. |
+ | <WRAP round download> | ||
+ | **Resources: | ||
+ | * Fritzing files: [[downgit> | ||
+ | * LTspice files: [[downgit> | ||
+ | </ | ||
==== For Further reading: ==== | ==== For Further reading: ==== | ||
Output Stages [[http:// | Output Stages [[http:// | ||
[[http:// | [[http:// | ||
+ | |||
+ | |||
**Return to Lab Activity [[university: | **Return to Lab Activity [[university: |