Wiki

This version is outdated by a newer approved version.DiffThis version (01 Jan 2021 16:16) was approved by Doug Mercer.The Previously approved version (01 Jan 2021 16:13) is available.Diff

This is an old revision of the document!


Activity: Making a full Operational Amplifier from previous blocks

High gain amplifier

Objective:

By combining the circuit blocks already explored, the goal is to build a complete high open loop gain amplifier from a few discrete devices.

Materials:

ADALM2000 Active Learning Module
Solder-less breadboard
Jumper wires
1 - 8.2KΩ Resistor (close approx. can be made by connecting your 1.5KΩ and 6.8KΩ in series)
1 - 47KΩ Resistor
1 - 100KΩ Resistor
2 - 470KΩ Resistor
1 - 10KΩ Resistor
1 - 1KΩ Resistor
2 - 22uF capacitor
1 - 1uF capacitor
1 - 47nF capacitor
1 - Small signal PNP transistors (2N3906)
3 - Small signal NPN transistors (2N3904 SSM2212)

Directions:

On your solder-less breadboard construct the amplifier circuit shown in figure 1 below. The breadboard connections are shown in figure 2. The green boxes indicate connections to the connector on ADALM2000.

Figure 1 Three stage amplifier

Hardware Setup:

Connect your circuit to the ADALM2000 I/O connector as indicated by the green boxes. It is best to ground the unused negative scope inputs when not being used. If the SSM2212 NPN matched pair is used then it is best to use it for Q1 and Q2.

Figure 2 Three stage amplifier Breadboard Circuit

Procedure:

Configure waveform generator for a 1 KHz sine wave with an amplitude of 400 mV peak-to-peak and zero offset. Using scope channel 1 to observe the input at W1 and scope channel 2 to observe the output of the amplifier at RL, record the input to output amplitude and phase relationship.

Figure 3 Three stage amplifier Waveforms

Questions:

What is the DC voltage seen at the base of Q1? What sets this DC level?

What is the gain from the input source, W1, to the output seen at RL? Which components set this gain and why?

Run a computer simulation of the amplifier and calculate the open loop gain as seen from the base of transistor Q1 to the output at the collector of Q4. Report this gain vs. frequency.

Change the value of the load resistor RL. How does lowering the value of RL affect the open loop and closed loop gain and why?

Change the value of compensation capacitor C3. How does raising and lowering the value of C3affect the frequency response and why?

What happens if C3 is completely removed and why?

What happens when C2is removed and why?

Unity gain amplifier

Objective:

By combining some of the circuit blocks already explored, the goal is to build a complete unity gain buffer amplifier. The addition of the current mirror load for the differential stage is a key improvement to this simple amplifier.

Materials:

ADALM2000 Active Learning Module
Solder-less breadboard
Jumper wires
1 - 15KΩ Resistor (a 10KΩ in series with a 4.7KΩ can be substituted)
2 - Small signal PNP transistors (2N3906, or SSM2220 PNP match pair can be used)
6 - Small signal NPN transistors (2N3904, use SSM2212 NPN matched pair for Q1 and Q2 A TIP31C may be substituted for Q5 if you don't have enough 2N3904 devices)

Directions:

Construct the circuit shown in figure 4 on your solder-less breadboard. The breadboard connections are shown in figure 5.

Figure 4 Amplifier with unity gain

Hardware Setup:

Connect your circuit to the ADALM2000 I/O connector as indicated by the green boxes. It is best to ground the unused negative scope inputs when not being used.

Figure 5 Amplifier with unity gain Breadboard Circuit

Procedure:

Configure AWG1 for a 1 KHz sine wave with an amplitude of 2 V peak-to-peak and zero offset. Using scope channel 1 to observe the input at W1 and scope channel 2 to observe the output of the amplifier, record the input to output amplitude and phase relationship.

Figure 6 Amplifier with unity gain Waveforms

Questions:

Add questions here:

Appendix: More advanced versions on a PC board

PC board design files for this experiment, and other related extentions, can be found on the ADI GitHub education tool repository. The PCB schematic is shown in figure 2 and a photo of the board is shown in figure 3.

Experiment board design files

Figure A1, Operational Amplifier PCB schematic.

The PCB uses the standard 8 pin DIP single op-amp footprint and can be inserted into a solder-less breadboard.

Figure A2, Operational Amplifier PC Board.

Resources:

Return to Lab Activity Table of Contents

university/courses/electronics/electronics-lab-13.1609514186.txt.gz · Last modified: 01 Jan 2021 16:16 by Doug Mercer