Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
university:courses:electronics:electronics-lab-12m [12 Jul 2019 13:38]
andreeapop [Activity 12M. MOS Differential pair]
university:courses:electronics:electronics-lab-12m [23 Aug 2019 13:07] (current)
amiclaus
Line 39: Line 39:
 <WRAP centeralign>​ Figure 3 NMOS Differential pair Breadboard Circuit </​WRAP>​ <WRAP centeralign>​ Figure 3 NMOS Differential pair Breadboard Circuit </​WRAP>​
  
-The first waveform generator should be configured for a 200 Hz Triangle wave with 4 volt amplitude and 0 offset. The second generator should be configured also for a 200 Hz Triangle wave with 4 volts amplitude and 0 volts offset but with 180 degree phase. Channel one of the scope should be connected with 1+ to the output of the first generator, W1 and 1- connected to W2. Channel 2 should be connected to display 2+ and 2- and set to 1 V per division.+The first waveform generator should be configured for a 200 Hz Triangle wave with 4 volt amplitude ​peak-to-peak ​and 0 offset. The second generator should be configured also for a 200 Hz Triangle wave with 4 volts amplitude ​peak-to-peak ​and 0 volts offset but with 180 degree phase. Channel one of the scope should be connected with 1+ to the output of the first generator, W1 and 1- connected to W2. Channel 2 should be connected to display 2+ and 2- and set to 1 V per division.
  
 ===== Procedure: ===== ===== Procedure: =====
university/courses/electronics/electronics-lab-12m.txt · Last modified: 23 Aug 2019 13:07 by amiclaus