Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Last revisionBoth sides next revision
university:courses:electronics:electronics-lab-12m [12 Jul 2019 13:38] – [Activity 12M. MOS Differential pair] Pop Andreeauniversity:courses:electronics:electronics-lab-12m [23 Aug 2019 13:07] Antoniu Miclaus
Line 39: Line 39:
 <WRAP centeralign> Figure 3 NMOS Differential pair Breadboard Circuit </WRAP> <WRAP centeralign> Figure 3 NMOS Differential pair Breadboard Circuit </WRAP>
  
-The first waveform generator should be configured for a 200 Hz Triangle wave with 4 volt amplitude and 0 offset. The second generator should be configured also for a 200 Hz Triangle wave with 4 volts amplitude and 0 volts offset but with 180 degree phase. Channel one of the scope should be connected with 1+ to the output of the first generator, W1 and 1- connected to W2. Channel 2 should be connected to display 2+ and 2- and set to 1 V per division.+The first waveform generator should be configured for a 200 Hz Triangle wave with 4 volt amplitude peak-to-peak and 0 offset. The second generator should be configured also for a 200 Hz Triangle wave with 4 volts amplitude peak-to-peak and 0 volts offset but with 180 degree phase. Channel one of the scope should be connected with 1+ to the output of the first generator, W1 and 1- connected to W2. Channel 2 should be connected to display 2+ and 2- and set to 1 V per division.
  
 ===== Procedure: ===== ===== Procedure: =====
university/courses/electronics/electronics-lab-12m.txt · Last modified: 25 Jun 2020 22:07 by 127.0.0.1