Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision |
university:courses:electronics:electronics-lab-12 [12 Jul 2019 13:38] – [Activity 12. BJT Differential pair] Pop Andreea | university:courses:electronics:electronics-lab-12 [25 Jun 2020 22:07] (current) – external edit 127.0.0.1 |
---|
<WRAP centeralign> Figure 3 Differential pair with tail resistor Breadboard Circuit </WRAP> | <WRAP centeralign> Figure 3 Differential pair with tail resistor Breadboard Circuit </WRAP> |
| |
The first waveform generator should be configured for a 200 Hz Triangle wave with 4 volts amplitude and 0 offset. The second generator should be configured also for a 200 Hz Triangle wave with 4 volts amplitude and 0 volts offset but with 180 degree phase. The resistor dividers will reduce the signal amplitude seen at the bases of Q<sub>1</sub>and Q<sub>2</sub>to slightly less than 200 mV. Channel one of the scope should be connected with 1+ to the output of the first generator, W1 and 1- connected to W2. Channel 2 should be connected to display 2+ and 2- and set to 1V per division. | The first waveform generator should be configured for a 200 Hz Triangle wave with 4 volts amplitude peak-to-peak and 0 offset. The second generator should be configured also for a 200 Hz Triangle wave with 4 volts amplitude peak-to-peak and 0 volts offset but with 180 degree phase. The resistor dividers will reduce the signal amplitude seen at the bases of Q<sub>1</sub>and Q<sub>2</sub>to slightly less than 200 mV. Channel one of the scope should be connected with 1+ to the output of the first generator, W1 and 1- connected to W2. Channel 2 should be connected to display 2+ and 2- and set to 1V per division. |
| |
===== Procedure: ===== | ===== Procedure: ===== |
<WRAP round download> | <WRAP round download> |
**Resources:** | **Resources:** |
* Fritzing files: [[ https://minhaskamal.github.io/DownGit/#/home?url=https://github.com/analogdevicesinc/education_tools/tree/master/m2k/fritzing/bjt_diff_pair_bb | bjt_diff_pair_bb ]] | * Fritzing files: [[downgit>education_tools/tree/master/m2k/fritzing/bjt_diff_pair_bb | bjt_diff_pair_bb ]] |
* LTspice files: [[ https://minhaskamal.github.io/DownGit/#/home?url=https://github.com/analogdevicesinc/education_tools/tree/master/m2k/ltspice/bjt_diff_pair_ltspice | bjt_diff_pair_ltspice ]] | * LTspice files: [[downgit>education_tools/tree/master/m2k/ltspice/bjt_diff_pair_ltspice | bjt_diff_pair_ltspice ]] |
</WRAP> | </WRAP> |
| |