This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:courses:electronics:electronics-lab-12 [05 Sep 2017 14:43] – add breadboard circuits + plots Antoniu Miclaus | university:courses:electronics:electronics-lab-12 [25 Jun 2020 22:07] (current) – external edit 127.0.0.1 | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== Activity | + | ====== Activity: BJT Differential pair ====== |
===== Objective: ===== | ===== Objective: ===== | ||
Line 38: | Line 38: | ||
<WRAP centeralign> | <WRAP centeralign> | ||
- | The first waveform generator should be configured for a 200 Hz Triangle wave with 4 volts amplitude and 0 offset. The second generator should be configured also for a 200 Hz Triangle wave with 4 volts amplitude and 0 volts offset but with 180 degree phase. The resistor dividers will reduce the signal amplitude seen at the bases of Q< | + | The first waveform generator should be configured for a 200 Hz Triangle wave with 4 volts amplitude |
===== Procedure: ===== | ===== Procedure: ===== | ||
Line 106: | Line 106: | ||
Repeat the common mode gain measurements on the circuit shown in figure 3 with the tail current source. How has the result changed and why. | Repeat the common mode gain measurements on the circuit shown in figure 3 with the tail current source. How has the result changed and why. | ||
+ | |||
+ | <WRAP round download> | ||
+ | **Resources: | ||
+ | * Fritzing files: [[downgit> | ||
+ | * LTspice files: [[downgit> | ||
+ | </ | ||
**Return to Lab Activity [[university: | **Return to Lab Activity [[university: | ||