This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-12 [05 Mar 2019 12:27] – [Questions:] Antoniu Miclaus | university:courses:electronics:electronics-lab-12 [23 Aug 2019 13:07] – Antoniu Miclaus | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== Activity | + | ====== Activity: BJT Differential pair ====== |
===== Objective: ===== | ===== Objective: ===== | ||
Line 38: | Line 38: | ||
<WRAP centeralign> | <WRAP centeralign> | ||
- | The first waveform generator should be configured for a 200 Hz Triangle wave with 4 volts amplitude and 0 offset. The second generator should be configured also for a 200 Hz Triangle wave with 4 volts amplitude and 0 volts offset but with 180 degree phase. The resistor dividers will reduce the signal amplitude seen at the bases of Q< | + | The first waveform generator should be configured for a 200 Hz Triangle wave with 4 volts amplitude |
===== Procedure: ===== | ===== Procedure: ===== |