university:courses:electronics:electronics-lab-12 [05 Mar 2019 12:27]
Antoniu Miclaus [Questions:]
university:courses:electronics:electronics-lab-12 [23 Aug 2019 13:07]
Antoniu Miclaus
Line 1: Line 1:
-====== Activity ​12. BJT Differential pair ======+====== ActivityBJT Differential pair ======
  
 ===== Objective: ===== ===== Objective: =====
Line 38: Line 38:
 <WRAP centeralign>​ Figure 3 Differential pair with tail resistor Breadboard Circuit </​WRAP>​ <WRAP centeralign>​ Figure 3 Differential pair with tail resistor Breadboard Circuit </​WRAP>​
  
-The first waveform generator should be configured for a 200 Hz Triangle wave with 4 volts amplitude and 0 offset. The second generator should be configured also for a 200 Hz Triangle wave with 4 volts amplitude and 0 volts offset but with 180 degree phase. The resistor dividers will reduce the signal amplitude seen at the bases of Q<​sub>​1</​sub>​and Q<​sub>​2</​sub>​to slightly less than 200 mV. Channel one of the scope should be connected with 1+ to the output of the first generator, W1 and 1- connected to W2. Channel 2 should be connected to display 2+ and 2- and set to 1V per division.+The first waveform generator should be configured for a 200 Hz Triangle wave with 4 volts amplitude ​peak-to-peak ​and 0 offset. The second generator should be configured also for a 200 Hz Triangle wave with 4 volts amplitude ​peak-to-peak ​and 0 volts offset but with 180 degree phase. The resistor dividers will reduce the signal amplitude seen at the bases of Q<​sub>​1</​sub>​and Q<​sub>​2</​sub>​to slightly less than 200 mV. Channel one of the scope should be connected with 1+ to the output of the first generator, W1 and 1- connected to W2. Channel 2 should be connected to display 2+ and 2- and set to 1V per division.
  
 ===== Procedure: ===== ===== Procedure: =====
university/courses/electronics/electronics-lab-12.txt · Last modified: 25 Jun 2020 22:07 (external edit)