Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
university:courses:electronics:electronics-lab-11m [05 Mar 2019 12:26]
amiclaus [Procedure:]
university:courses:electronics:electronics-lab-11m [23 Aug 2019 13:06]
amiclaus
Line 1: Line 1:
-====== Activity ​11M. The Source follower (NMOS)======+====== ActivityThe Source follower (NMOS)======
  
 ===== Objective: ===== ===== Objective: =====
Line 26: Line 26:
 <WRAP centeralign>​ Figure 2 Source Follower Breadboard Circuit </​WRAP>​ <WRAP centeralign>​ Figure 2 Source Follower Breadboard Circuit </​WRAP>​
  
-The waveform generator should be configured for a 1 KHz Sine wave with 4 volt amplitude and 0 offset. The Single ended input of scope channel 2 (2+) is used to measure the voltage at the source. The Scope configured with channel 1+ connected to display the AWG generator output. When measuring the input to output error, channel 2 of the scope should be connected to display 2+ and 2- differential.+The waveform generator should be configured for a 1 KHz Sine wave with 4 volt amplitude ​peak-to-peak ​and 0 offset. The Single ended input of scope channel 2 (2+) is used to measure the voltage at the source. The Scope configured with channel 1+ connected to display the AWG generator output. When measuring the input to output error, channel 2 of the scope should be connected to display 2+ and 2- differential.
  
 ===== Procedure: ===== ===== Procedure: =====
Line 94: Line 94:
 <WRAP centeralign>​ Figure 8 Output Impedance Test Breadboard Circuit </​WRAP>​ <WRAP centeralign>​ Figure 8 Output Impedance Test Breadboard Circuit </​WRAP>​
  
-The waveform generator should be configured for a 1 KHz Sine wave with 2 volt amplitude with the offset set equal to minus the V<​sub>​GS</​sub>​ of M<​sub>​1</​sub>​ ( approximately -V ). This injects a +/- 0.1mA (1V/10KΩ) current into M<​sub>​1</​sub>'​s source. Scope input 2+ measures the change in voltage seen at the source.+The waveform generator should be configured for a 1 KHz Sine wave with 2 volt amplitude ​peak-to-peak ​with the offset set equal to minus the V<​sub>​GS</​sub>​ of M<​sub>​1</​sub>​ ( approximately -V ). This injects a +/- 0.1mA (1V/10KΩ) current into M<​sub>​1</​sub>'​s source. Scope input 2+ measures the change in voltage seen at the source.
  
 ===== Procedure: ===== ===== Procedure: =====
university/courses/electronics/electronics-lab-11m.txt · Last modified: 23 Aug 2019 13:06 by amiclaus