This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-10 [23 Mar 2017 16:16] – [Materials:] Doug Mercer | university:courses:electronics:electronics-lab-10 [24 Jul 2017 15:25] – change amplitude value to peak-peak Antoniu Miclaus | ||
---|---|---|---|
Line 25: | Line 25: | ||
===== Hardware Setup: ===== | ===== Hardware Setup: ===== | ||
- | Waveform generator W1 should be configured for a 1 KHz triangle wave with 2 volt amplitude and 2V offset. The Single ended input of scope channel 2 (2+) is used to measure the regulated output voltage at the collector of Q< | + | Waveform generator W1 should be configured for a 1 KHz triangle wave with 4 volt amplitude and 2V offset. The Single ended input of scope channel 2 (2+) is used to measure the regulated output voltage at the collector of Q< |
===== Procedure: ===== | ===== Procedure: ===== |