This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-10 [05 Mar 2019 12:26] – [Using an NPN transistor array:] Antoniu Miclaus | university:courses:electronics:electronics-lab-10 [23 Aug 2019 13:05] – Antoniu Miclaus | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== Activity | + | ====== Activity: Shunt regulator ====== |
===== Objective: ===== | ===== Objective: ===== | ||
Line 29: | Line 29: | ||
<WRAP centeralign> | <WRAP centeralign> | ||
- | Waveform generator W1 should be configured for a 1 KHz triangle wave with 4 volt amplitude and 2V offset. The Single ended input of scope channel 2 (2+) is used to measure the regulated output voltage at the collector of Q< | + | Waveform generator W1 should be configured for a 1 KHz triangle wave with 4 volt amplitude |
===== Procedure: ===== | ===== Procedure: ===== |