Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision Both sides next revision
university:courses:electronics:comms-lab-pulse-osc [24 Jul 2017 16:29]
Antoniu Miclaus change amplitude value to peak-peak
university:courses:electronics:comms-lab-pulse-osc [04 Jan 2018 07:49]
Trecia Agoylo
Line 43: Line 43:
 =====Hardware Setup:===== =====Hardware Setup:=====
  
-Setup AWG1 as a square wave with 1.4V amplitude and zero offset. Set the frequency to 50 KHz and the duty cycle to 70% ( square wave high for 70% of the period ). Set both scope inputs to 500 mV/div and the time base to uSec/div. Set the trigger on the falling edge of channel 1.+Setup AWG1 as a square wave with 1.4V amplitude and zero offset. Set the frequency to 50 KHz and the duty cycle to 50% ( square wave high for 50% of the period ). Set both scope inputs to 500 mV/div and the time base to uSec/div. Set the trigger on the falling edge of channel 1. 
 + 
 +{{ :​university:​courses:​electronics:​apulse_bb.png?​ |}} 
 + 
 +<WRAP centeralign>​ Figure 3 Pulsed oscillator circuit breadboard connections </​WRAP>​
  
 =====Procedure:​===== =====Procedure:​=====
  
 Turn on the +5V power supply and start the AWG. Observe the output waveform. It should consist of a burst of a few cycles of sinewave starting at the falling edge of the AWG 1 square wave and ending on the rising edge.  ​ Turn on the +5V power supply and start the AWG. Observe the output waveform. It should consist of a burst of a few cycles of sinewave starting at the falling edge of the AWG 1 square wave and ending on the rising edge.  ​
 +{{ :​university:​courses:​electronics:​apulse_scopyshot.png?​ |}}
 +
 +<WRAP centeralign>​ Figure 4 Pulsed oscillator circuit Scopy shot</​WRAP>​
 +
  
 Notice that the output sine wave swings positive and negative around ground (0 V). Measure the frequency of the output sinewave. Measure the peak to peak amplitude of the first and last cycle of the output sinewave burst. How much has the amplitude fallen off from the start to the end of the burst? Notice that the output sine wave swings positive and negative around ground (0 V). Measure the frequency of the output sinewave. Measure the peak to peak amplitude of the first and last cycle of the output sinewave burst. How much has the amplitude fallen off from the start to the end of the burst?
university/courses/electronics/comms-lab-pulse-osc.txt · Last modified: 25 Jun 2020 22:07 (external edit)