Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Next revision
Previous revision
university:courses:electronics:comms-lab-lfsr [04 Aug 2014 14:39]
Doug Mercer created
university:courses:electronics:comms-lab-lfsr [27 Mar 2017 17:17]
Doug Mercer [Procedure:]
Line 18: Line 18:
  
 =====Materials:​===== =====Materials:​=====
- +ADALM2000 Active Learning Module\\
-Analog Discovery Lab hardware\\+
 Solder-less breadboard\\ Solder-less breadboard\\
 Jumper wires\\ Jumper wires\\
Line 29: Line 28:
 Build the linear feedback shift register circuit shown in figure 1, preferably on your solder-less breadboard. The CD4035 4 bit shift register is shown but another similar shift register with parallel outputs could be substituted. A two input XOR gate can also be constructed using the CD4007 CMOS transistor array as shown in the lab activity on the [[university:​courses:​electronics:​electronics-lab-30|transmission gate XOR]]. Build the linear feedback shift register circuit shown in figure 1, preferably on your solder-less breadboard. The CD4035 4 bit shift register is shown but another similar shift register with parallel outputs could be substituted. A two input XOR gate can also be constructed using the CD4007 CMOS transistor array as shown in the lab activity on the [[university:​courses:​electronics:​electronics-lab-30|transmission gate XOR]].
  
-Connect the D0-D3 digital inputs and the D5 digital output on the Analog Discovery ​connector and the positive 5 volt power and ground to the circuit as shown.+Connect the D0-D3 digital inputs and the D5 digital output on the ADALM2000 ​connector and the positive 5 volt power and ground to the circuit as shown.
  
 {{ :​university:​courses:​electronics:​alfsr_f1.png?​500 |}} {{ :​university:​courses:​electronics:​alfsr_f1.png?​500 |}}
Line 41: Line 40:
 =====Procedure:​===== =====Procedure:​=====
  
-Start the Waveforms ​software. Open power supply control window and turn on the fixed 5 Volt power supply, VP+. Open up the Digital Pattern Generator screen. Add a signal. Select DIO 5. Set the type to clock. You should see something that looks like the screen below in figure 2. Lastly, hit the Run button. +Start the Scopy software. Open power supply control window and turn on the +5 Volt power supply, VP+. Open up the Digital Pattern Generator screen. Add a signal. Select DIO 5. Set the type to clock. You should see something that looks like the screen below in figure 2. Lastly, hit the Run button.
- +
-{{ :​university:​courses:​electronics:​alfsr_f2.jpg?​500 |}}+
  
 <WRAP centeralign>​ Figure 2 Digital pattern generator screen. </​WRAP>​ <WRAP centeralign>​ Figure 2 Digital pattern generator screen. </​WRAP>​
  
-Open the edit signal parameters window ​by clicking on the little blue pencil icon. Make sure the type is set to clock and the output is set to PP (push-pull). Set the frequency to 5 KHz. With the Duty cycle set to 50%.+Open the edit signal parameters window. Make sure the type is set to clock and the output is set to PP (push-pull). Set the frequency to 5 KHz. With the Duty cycle set to 50%.
  
 Open the logic analyzer window and add a bus signal for DIO 0-3. Check the show as analog box when you make the bus. Hit the Run button. You should see a random sequence something like what is shown in figure 3. Notice that the pattern repeats every 15 clocks. Open the logic analyzer window and add a bus signal for DIO 0-3. Check the show as analog box when you make the bus. Hit the Run button. You should see a random sequence something like what is shown in figure 3. Notice that the pattern repeats every 15 clocks.
- 
-{{ :​university:​courses:​electronics:​alfsr_f3.jpg?​500 |}} 
  
 <WRAP centeralign>​ Figure 3 Logic Analyzer screen. </​WRAP>​ <WRAP centeralign>​ Figure 3 Logic Analyzer screen. </​WRAP>​
university/courses/electronics/comms-lab-lfsr.txt · Last modified: 27 Mar 2017 17:17 by Doug Mercer