Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

university:courses:electronics:comms-lab-clapp-osc [27 Mar 2017 17:11]
Doug Mercer [Materials:]
university:courses:electronics:comms-lab-clapp-osc [25 Jun 2020 22:07]
Line 1: Line 1:
-======Activity:​ The Clapp Oscillator====== 
- 
-=====Objective:​===== 
- 
-Oscillators come in many forms. In this lab activity we will explore the Clapp configuration which uses a taped capacitor divider to provide the feedback path and a series LC resonator. 
- 
-=====Background:​===== 
- 
-A Clapp oscillator is in effect a series tuned version of the Colpitts oscillator. The Clapp oscillator is much like a Colpitts oscillator with the capacitive voltage divider producing the feedback signal. The addition of a capacitor C<​sub>​3</​sub>​ in series with the inductor L<​sub>​1</​sub>​ results in the difference in the two designs and distinguishes the Clapp Oscillator from the Colpitts and Hartley configurations. As with all oscillators,​ the Barkhausen criteria must be adhered to requiring a total gain of one and a phase shift of zero degrees from input to output. 
-The frequency of oscillation can be calculated in the same way as any resonant circuit, using: 
- 
-{{ :​university:​courses:​electronics:​ata1_e1.png?​200 |}} 
- 
-Ignoring the transistor capacitive effect between the base and collector, the resonant frequency may be calculated using the total equivalent capacitance (C<​sub>​TOT</​sub>​) given by: 
- 
-{{ :​university:​courses:​electronics:​aclap-osc_e2.png?​200 |}} 
- 
-Figure 1 shows a typical Clapp oscillator. The frequency determining series resonant tuned circuit is formed by L<​sub>​1</​sub>​ and C<​sub>​TOT</​sub>​ and is used as the collector load impedance of the common base amplifier Q<​sub>​1</​sub>​. A large inductance, L<​sub>​2</​sub>,​ provides a DC path for the collector current while presenting a high impedance at the resonate frequency. This gives the amplifier a high gain only at the resonant frequency. This configuration of the Hartley oscillator uses a common base amplifier, the base of Q<​sub>​1</​sub>​is biased to an appropriate DC level by resistor divider R<​sub>​1</​sub>​ and R<​sub>​2</​sub>​ but is connected directly to an AC ground by C<​sub>​4</​sub>​. In the common base mode the output voltage waveform at the collector, and the input signal at the emitter are in phase. This ensures that the fraction of the output signal from the node between C<​sub>​1</​sub>​ and C<​sub>​2</​sub>,​ fed back from the tuned collector load to the emitter provides the required positive feedback. ​ 
- 
-{{ :​university:​courses:​electronics:​aclap-osc_f1.png?​530 |}} 
- 
-<WRAP centeralign>​ Figure 1, Basic Clapp Oscillator </​WRAP>​ 
- 
-The combination of C<​sub>​1</​sub>​and C<​sub>​2</​sub>​ also forms a low frequency time constant with the emitter resistor R<​sub>​3</​sub>​ to provide an average DC voltage level proportional to the amplitude of the feedback signal at the emitter of Q<​sub>​1</​sub>​. This provides automatic control of the gain of the amplifier to give the closed loop gain of 1 required by the oscillator. The emitter resistor R<​sub>​3</​sub>​ is not decoupled because the emitter node is used as the common base amplifier input. The base is connected to AC ground by C<​sub>​4</​sub>,​ which will provide a very low reactance at the oscillator frequency. 
- 
-====Pre Lab Simulations==== 
- 
-Build a simulation schematic of the Clapp oscillator as shown in figure 1. Calculate values for bias resistors R<​sub>​1</​sub>​ and R<​sub>​2</​sub>​ such that with emitter resistor R<​sub>​3</​sub>​set to 500 Ω, the collector current in NPN transistor Q<​sub>​1</​sub>​ is approximately 1 mA. Assume the circuit is powered from a +10V power supply. Be sure to keep the sum of R<​sub>​1</​sub>​ and R<​sub>​2</​sub>​ ( total resistance greater than 10 KΩ) has high as practical to keep the standing current in the resistor divider as low as practical. Remember that C<​sub>​4</​sub>​ provides an AC ground at the base of Q<​sub>​1</​sub>​. Set base decoupling capacitor C<​sub>​4</​sub>​ and output AC coupling capacitor C<​sub>​5</​sub>​ to 0.1uF. Calculate a value for L<​sub>​1</​sub>​ such that the resonate frequency, with C<​sub>​1</​sub>​ set equal to 1nF and C<​sub>​2</​sub>​ set to 1 nF, will be close to 750 KHz. Use a high value for L<​sub>​3</​sub>​ of at least 10 mH. Perform a transient simulation. Save these results to compare with the measurements you take on the actual circuit and to include with your lab report. 
- 
-=====Materials:​===== 
-ADALM2000 Active Learning Module\\ 
-Solder-less breadboard, and jumper wire kit\\ 
-1 - 2N3904 NPN transistor\\ 
-1 - 1 uH inductor\\ 
-1 - 10 uH inductor\\ 
-1 - 100 uH inductor\\ 
-1 - 10 mH inductor ( L<​sub>​3</​sub>​ )\\ 
-1 - 1 nF capacitor ( C<​sub>​1</​sub>​ )\\ 
-1 - 4.7 nF capacitor ( C<​sub>​2</​sub>​ )\\ 
-2 - 0.1 uF capacitors ( marked 104 )\\ 
-1 - 470 Ω resistor ( R<​sub>​3</​sub>​)\\ 
-Other resistor, capacitors and inductors as needed 
- 
-=====Directions:​===== 
- 
-Build the Clapp Oscillator shown in figure 2 using your solder-less breadboard. Pick standard values from your parts kit for bias resistors R<​sub>​1</​sub>​ and R<​sub>​2</​sub>​ such that with emitter resistor R<​sub>​3</​sub>​set to 470 Ω, the collector current in NPN transistor Q<​sub>​1</​sub>​ is approximately 1 mA. Start with C<​sub>​1</​sub>​ = 1 nF and C<​sub>​2</​sub>​ = 4.7 nF. The frequency of the oscillator can be from around 500 KHz to 2 MHz depending on the values chosen for C<​sub>​1</​sub>,​ C<​sub>​2</​sub>,​ C<​sub>​3</​sub>​ and L<​sub>​1</​sub>​. ​ Calculate a value for C<​sub>​3</​sub>​ and pick the closest value from your parts kit. This oscillator circuit can produce a sine wave output in excess of 10 Vpp at an approximate frequency set by the value chosen for L<​sub>​1</​sub>​. ​ 
- 
-{{ :​university:​courses:​electronics:​aclap-osc_f2.png?​530 |}} 
- 
-<WRAP centeralign>​ Figure 2 Clapp Oscillator </​WRAP>​ 
- 
-=====Hardware Setup:===== 
- 
-The green squares indicate where to connect the Discovery module AWG, scope channels and power supplies. Be sure to only turn on the power supplies after you double check your wiring. 
- 
-=====Procedure:​===== 
- 
-Having finished construction the Clapp oscillator check that the circuit is oscillating correctly by turning on both the + and - 5 V power supplies and connecting one of the oscilloscope channels to the output terminal. It may be found that the value of R<​sub>​3</​sub>​ is fairly critical, producing either a large distorted waveform or an intermittent low or no output. To find the best value for R<​sub>​3</​sub>,​ it could be replaced by a 1 KΩ potentiometer for experimentation to find the value that gives the best wave shape and reliable amplitude. 
- 
-=====Questions:​===== 
- 
-Measure the peak to peak output voltage of the output. Measure the DC ( average ) level of the output waveform at the collector of Q<​sub>​1</​sub>​ and on the other (output) side of AC coupling capacitor C<​sub>​4</​sub>​. Measure the voltage at the emitter of Q<​sub>​1</​sub>​. Calculate the average emitter current by measuring the voltage across R<​sub>​3</​sub>​. Compare your measurements with your calculations and simulations. Measure the period (time T) of the output waveform and its frequency (1/T). Compare this measured frequency to what you calculated by:\\ 
-<​m>​F_R = 1 / {2 pi sqrt(LC)}</​m>​. 
- 
-Fill in the table below with the measured frequency for other L<​sub>​1</​sub>​ values for two different values of C<​sub>​3</​sub>​. Use the values in the table as suggested options but try to include as many different values as possible using series and parallel combinations of the inductors supplied in your parts kit. Any of the L<​sub>​1</​sub>​ optional values shown below should give reliable oscillation. 
- 
-^L<​sub>​1</​sub>​ Options^C<​sub>​1</​sub>​ = 1nF L<​sub>​2</​sub>​ = 4.7nF ^C<​sub>​1</​sub>​ = 10nF C<​sub>​2</​sub>​ = 1nF^ 
-|Value|Frequency with C<​sub>​3</​sub>​= ?|Frequency with C<​sub>​3</​sub>​= ?| 
-|10 uH|  |  | 
-|20 uH|  |  | 
-|50 uH|  |  | 
-|100 uH|  |  | 
- 
-**For Further Reading:** 
- 
-http://​en.wikipedia.org/​wiki/​Clapp_oscillator\\ 
-http://​en.wikipedia.org/​wiki/​Barkhausen_stability_criterion\\ 
- 
-**Return to Lab Activity [[university:​courses:​electronics:​labs|Table of Contents]].** 
- 
  
university/courses/electronics/comms-lab-clapp-osc.txt · Last modified: 25 Jun 2020 22:07 (external edit)