This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:courses:electronics:circuitsimulationnotes [11 May 2014 20:57] – [Software Links:] Doug Mercer | university:courses:electronics:circuitsimulationnotes [01 Nov 2018 13:34] – add LTspice doc + lab files Antoniu Miclaus | ||
---|---|---|---|
Line 16: | Line 16: | ||
The archive files contain folders with one or more example schematics for use with each Lab Activity. A few extra device model files are also included in the archive that do not generally come bundled with the software. These can be added to the model library by dragging and dropping them onto the SIMetrix main window. The provided schematic files are also compatible with the Analog Devices supplied ADsimPE< | The archive files contain folders with one or more example schematics for use with each Lab Activity. A few extra device model files are also included in the archive that do not generally come bundled with the software. These can be added to the model library by dragging and dropping them onto the SIMetrix main window. The provided schematic files are also compatible with the Analog Devices supplied ADsimPE< | ||
+ | |||
+ | There is also an archive file that contains schematic files with examples for the lab activities that are compatible with the LTspice< | ||
It is recommended that the free introductory version of SIMetrix (or ADsimPE) be installed on the students' | It is recommended that the free introductory version of SIMetrix (or ADsimPE) be installed on the students' | ||
- | **Electronics I lab simulation schematic files:** | + | **Electronics I lab simulation schematic files with ADsimPE:** |
{{: | {{: | ||
- | **Electronics II lab simulation schematic files:** | + | **Electronics II lab simulation schematic files with ADsimPE:** |
{{: | {{: | ||
+ | |||
+ | **Electronics lab simulation schematic files with LTspice:** | ||
+ | [[https:// | ||
**Mini-Tutorial on analog circuit simulation: | **Mini-Tutorial on analog circuit simulation: | ||
Line 45: | Line 50: | ||
http:// | http:// | ||
+ | |||
+ | [5] **LTspice** is a freeware computer software implementing a SPICE simulator of electronic circuits, produced by semiconductor manufacturer Linear Technology, now part of Analog Devices. | ||
+ | |||
+ | http:// | ||
[2] **Fritzing** is an open-source hardware initiative that makes electronics accessible as a creative material for anyone. | [2] **Fritzing** is an open-source hardware initiative that makes electronics accessible as a creative material for anyone. | ||
http:// | http:// | ||
+ | |||
+ | |||
Another public domain circuit simulation software package:\\ | Another public domain circuit simulation software package:\\ |