Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
university:courses:electronics:buck_converter_basics [10 May 2019 20:16]
Mark Thoren add round download box [Slide Deck]
university:courses:electronics:buck_converter_basics [26 Mar 2020 00:38]
Mark Thoren Add references to ADALM-BUCK board.
Line 39: Line 39:
 Solder-less breadboard and jumper wire kit or Perma Proto solder breadboard\\ Solder-less breadboard and jumper wire kit or Perma Proto solder breadboard\\
 ADALP2000 parts kit parts as required\\ ADALP2000 parts kit parts as required\\
 +Optional: [[university:​tools:​lab_hw:​adalm_buck|ADALM-BUCK-ARDZ Module]]\\
 12V power supply (preferred) or 5V USB power supply (workable)\\ 12V power supply (preferred) or 5V USB power supply (workable)\\
 Voltmeter (optional, can use M2K in Voltmeter mode.)\\ Voltmeter (optional, can use M2K in Voltmeter mode.)\\
Line 145: Line 146:
 ==== Circuit Construction and Testing ==== ==== Circuit Construction and Testing ====
 Build the following breadboard circuit for the buck converter, following the schematic in Figure 16. (Q1, R2, R3 can be added later.) Note that the HPH1-1400L has six inductors that can be connected in any way (series, parallel, or a combination of the two). Be sure to observe proper polarity, connecting all inductors in series as shown. Build the following breadboard circuit for the buck converter, following the schematic in Figure 16. (Q1, R2, R3 can be added later.) Note that the HPH1-1400L has six inductors that can be connected in any way (series, parallel, or a combination of the two). Be sure to observe proper polarity, connecting all inductors in series as shown.
 +<WRAP info>
 +The circuits in this lab are compatible with solderless breadboard construction. However they are relatively complicated and take time to construct and debug. The [[university:​tools:​lab_hw:​adalm_buck|ADALM-BUCK-ARDZ Module]] is available as an alternative.
 +</​WRAP>​
  
 {{ :​university:​courses:​electronics:​buck_basics:​lt1054_2_to_1_bb.png |}} {{ :​university:​courses:​electronics:​buck_basics:​lt1054_2_to_1_bb.png |}}
university/courses/electronics/buck_converter_basics.txt · Last modified: 25 Jun 2020 22:07 (external edit)