Wiki

This version is outdated by a newer approved version.DiffThis version (30 Dec 2020 15:02) was approved by Robin Getz.The Previously approved version (25 May 2020 14:59) is available.Diff

This is an old revision of the document!


Circuits I & II

These course materials combine techniques for the analysis and simulation of linear electric circuits, and measurements of their properties. Topics include resistive and energy-storage circuit elements, controlled sources and operational amplifiers, systematic analysis methods, AC steady state, power systems, magnetic coupling and transformers, transients, frequency response, and Laplace transform and computer simulation methods using LTspice. Circuit analysis techniques such as Kirchhoff’s Laws, node voltages, and mesh currents. Thevenin and Norton equivalent circuits, sinusoidal steady state and phasors.

The textbooks and teaching materials provided on this wiki are considered open source and available for free use in non-commercial educational and academic settings. The only requirement is that they continue to retain the attribution to Analog Devices Inc. Supplying them on the ADI wiki allows registered users to contribute to the materials posted here improving the content and keeping them up to date.

Table of Contents:

The following are suggested topics selected from Wikipedia and Khan Academy

Circuits I

Circuits II

Title
Chapter 1 - Operational AmplifiersIdeal Voltage Feedback (VFB) Op Amp
Inverting Amplifier
Inverting Summing Amplifier
Chapter 2 - RC and L/R Time ConstantsRC circuits
RC time constant
RL circuits
RLC circuits
LC circuits
Chapter 3 - Reactance and Impedance - Inductive
Chapter 4 - Reactance And Impedance - Capacitive
Chapter 5 - Reactance And Impedance - R, L, And C
Chapter 6 - ResonanceElectrical resonance
Chapter 8 - FiltersFilters
Low pass filter
High pass filter
Band pass filter
Chapter 9 - Transformers
Chapter 11 - Power FactorPower Factor

Circuits I & Circuits II Lab Exercises

Other Resources

Analog Device Supplied Content

Supplemental Reading

Definitions

Blogs and FAQs

Wikipedia

While Analog Devices is not responsible for, nor can it guarantee the accuracy of the content on Wikipedia, there might be value to the readers by providing links to topics related to the subjects covered in the above chapters as an Introduction to Electronics.

To that end, the following list is provided:

    1. linear elements
    1. nonlinear elements
  1. Active elements
    1. Darlington transistor (high current transistor configuration)
    2. Sziklai pair (high current transistor configuration, similar to Darlington pair)
    3. Operational amplifier applications – Common Op Amp configurations.
    4. Vacuum tube (“valves”)
      1. Brokaw bandgap reference – Another bandgap voltage reference topology.
    1. Switched-mode power supply (SMPS or “switching regulator”)
  2. Oscillator-related
    1. Latch (electronics)(like an SR latch)
      1. Amplifier circuit Schematic shows a differential amplifier with output tied to a common emitter amplifier that drives a class AB push–pull amplifier. In an example amplifier, we drive a similar push–pull output stage with a common collector (i.e., emitter follower) stage, and so our current amplifier will have no voltage gain.

End of Document

university/courses/circuits.1609336946.txt.gz · Last modified: 30 Dec 2020 15:02 by Robin Getz