This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
university:courses:alm1k:intro:oscilloscope-terminology [05 Apr 2021 19:01] Doug Mercer add duty cycle def |
university:courses:alm1k:intro:oscilloscope-terminology [06 Jun 2022 15:33] Doug Mercer fix spelling |
||
---|---|---|---|
Line 19: | Line 19: | ||
{{ :university:courses:alm1k:intro:intro-terminology-f1.png?600 |}} | {{ :university:courses:alm1k:intro:intro-terminology-f1.png?600 |}} | ||
- | ** Example Gird with Trace** | + | ** Example Grid with Trace** |
**Period (T):** | **Period (T):** | ||
Line 131: | Line 131: | ||
**Circuit Loading:** | **Circuit Loading:** | ||
- | The interaction of the oscilloscope input circuitry with the circuit being tested, distorting the signal. This is mostly due to the capacitance of the input but the input resistance can also be a factor in some cases. Loading – The unintentional interaction of the oscilloscope channel input impedance ( resistance and capacitance ) with the circuit being tested which distorts a signal. | + | The interaction of the oscilloscope input circuitry with the circuit being tested, distorting the signal. This is mostly due to the capacitance of the input but the input resistance can also be a factor in some cases. Loading – The unintentional interaction of the oscilloscope channel input impedance (resistance and capacitance) with the circuit being tested which distorts a signal. |
**Input Compensation:** | **Input Compensation:** | ||
- | An adjustment for passive attenuation scope frontends that balances the capacitance of the attenuator with the capacitance of the input circuitry. The ADALM2000 hardware includes trimmer capacitors internal on the circuit board. The ALICE desktop software does this frequency compensation using digital filters. | + | An adjustment for passive attenuation scope frontends that balances the capacitance of the attenuator with the capacitance of the input circuitry. The ADALM2000 hardware includes trimmer capacitors internal on the circuit board. The ALICE desktop software for the ADALM1000 does this frequency compensation using digital filters. |
**DC reference:** | **DC reference:** |