Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
university:courses:alm1k:circuits1:alm-cir-voltage-divider [22 Aug 2022 15:32]
Doug Mercer [Oscilloscope Probes:]
university:courses:alm1k:circuits1:alm-cir-voltage-divider [17 Jan 2023 15:34]
Doug Mercer [Experiment to compensate for the input capacitance of the ALM1000]
Line 37: Line 37:
  
 =====Experiment to compensate for the input capacitance of the ALM1000===== =====Experiment to compensate for the input capacitance of the ALM1000=====
 +
 +<​note>​The ADALM1000 (Rev. F version) has the ability to separate the voltage measurement connection from the voltage / current output pin, the Split I/O mode control in the AWG settings. The size of the parasitic capacitance is significantly different when using the CH A/B pins in Hi-Z mode vs using the AIN/BIN pins. The required external compensation capacitor value will be very different between the two pins. </​note>​
  
 ====Materials:​==== ====Materials:​====
university/courses/alm1k/circuits1/alm-cir-voltage-divider.txt · Last modified: 17 Jan 2023 15:34 by Doug Mercer