This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
university:courses:alm1k:circuits1:alm-cir-signal-generators [21 Oct 2021 15:37] – [Objective:] Doug Mercer | university:courses:alm1k:circuits1:alm-cir-signal-generators [07 Feb 2022 14:55] (current) – [General Notes:] Doug Mercer | ||
---|---|---|---|
Line 7: | Line 7: | ||
=====General Notes:===== | =====General Notes:===== | ||
- | As in all the ALM labs we use the following terminology when referring to the connections to the ALM1000 connector and configuring the hardware. The green shaded rectangles indicate connections to the ALM1000 analog I/O connector. The analog I/O channel pins are referred to as CA and CB. When configured to force voltage / measure current –V is added as in CA-V or when configured to force current | + | As in all the ALM labs we use the following terminology when referring to the connections to the ALM1000 connector and configuring the hardware. The green shaded rectangles indicate connections to the ALM1000 analog I/O connector. The analog I/O channel pins are referred to as CH A and CH B. The analog input only pins are referred to as AIN and BIN. |
- | + | ||
- | Scope traces | + | |
=====External Signal Source Options: | =====External Signal Source Options: |