This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
university:courses:alm1k:circuits1:alm-cir-envelope-detector [21 Mar 2018 17:42] Doug Mercer [Biased Envelope Detector] |
university:courses:alm1k:circuits1:alm-cir-envelope-detector [03 Jan 2021 22:12] Robin Getz fix links |
||
---|---|---|---|
Line 3: | Line 3: | ||
===== Objective: ===== | ===== Objective: ===== | ||
- | In this lab activity we will use the [[http://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/adalm1000.html|ADALM1000]] to introduce amplitude modulation (AM) and envelope detection demodulation. A signal's envelope is equivalent to its outline, and an envelope detector connects the amplitude peaks of the signal. [[university:courses:electronics:text:chapter-7#envelope_detector|Envelope detection]] has numerous applications in the fields of signal processing and communications, one of which is amplitude modulation (AM) detection or demodulation. | + | In this lab activity we will use the [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/adalm1000.html|ADALM1000]] to introduce amplitude modulation (AM) and envelope detection demodulation. A signal's envelope is equivalent to its outline, and an envelope detector connects the amplitude peaks of the signal. [[university:courses:electronics:text:chapter-7#envelope_detector|Envelope detection]] has numerous applications in the fields of signal processing and communications, one of which is amplitude modulation (AM) detection or demodulation. |
Amplitude modulation (AM) is a modulation technique used in electronic communication, most commonly for transmitting information via a radio frequency carrier wave. In amplitude modulation, the amplitude (signal strength) of the carrier wave is varied in proportion to the waveform being transmitted. That waveform may, for instance, correspond to the sounds to be reproduced by a loudspeaker, or the light intensity of television pixels. | Amplitude modulation (AM) is a modulation technique used in electronic communication, most commonly for transmitting information via a radio frequency carrier wave. In amplitude modulation, the amplitude (signal strength) of the carrier wave is varied in proportion to the waveform being transmitted. That waveform may, for instance, correspond to the sounds to be reproduced by a loudspeaker, or the light intensity of television pixels. | ||
Line 136: | Line 136: | ||
**For Further Reading:** | **For Further Reading:** | ||
- | * [[http://www.analog.com/en/technical-articles/integrated-diode-based-rf-detectors.html|Understanding, Operating, and Interfacing to Integrated Diode-Based RF Detectors]] | + | * [[adi>en/technical-articles/integrated-diode-based-rf-detectors.html|Understanding, Operating, and Interfacing to Integrated Diode-Based RF Detectors]] |
- | * [[http://www.analog.com/media/en/technical-documentation/application-notes/AN-423.pdf|Amplitude Modulation of the AD9850 Direct Digital Synthesizer]] | + | * [[adi>media/en/technical-documentation/application-notes/AN-423.pdf|Amplitude Modulation of the AD9850 Direct Digital Synthesizer]] |
- | * [[http://www.analog.com/en/analog-dialogue/raqs/raq-issue-92.html|Multipliers and Modulators]] | + | * [[adi>en/analog-dialogue/raqs/raq-issue-92.html|Multipliers and Modulators]] |
- | * [[http://www.analog.com/media/en/technical-documentation/data-sheets/ADL5511.pdf|Envelope and TruPwr RMS Detector | + | * [[adi>media/en/technical-documentation/data-sheets/ADL5511.pdf|Envelope and TruPwr RMS Detector |
]] | ]] | ||