Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
university:courses:alm1k:alm-lab-scr [07 Feb 2022 15:24]
Doug Mercer [Activity: Silicon Controlled Rectifiers (SCR)]
university:courses:alm1k:alm-lab-scr [27 May 2022 21:05]
Doug Mercer Spelling
Line 96: Line 96:
 ====LATCH-UP==== ====LATCH-UP====
  
-Latch-up is a potentially destructive situation in which a parasitic SCR is triggered, shorting the positive and negative supplies together. If current flow is not limited, electrical ​overstress ​will occur. The classic case of latch-up occurs in CMOS output devices, in which the driver transistors and wells form a four layer PNPN SCR structure when one of the two parasitic base-emitter junctions is momentarily forward biased during an overvoltage ​upset event. The SCR turns on and essentially causes a short between the V<​sub>​DD</​sub>​ power supply and ground.+Latch-up is a potentially destructive situation in which a parasitic SCR is triggered, shorting the positive and negative supplies together. If current flow is not limited, electrical ​over-stress ​will occur. The classic case of latch-up occurs in CMOS output devices, in which the driver transistors and wells form a four layer PNPN SCR structure when one of the two parasitic base-emitter junctions is momentarily forward biased during an over-voltage ​upset event. The SCR turns on and essentially causes a short between the V<​sub>​DD</​sub>​ power supply and ground.
  
 Since all these MOS devices are located close together on the monolithic die, with appropriate external excitation, the parasitic SCR devices may turn on, a behavior common with poorly designed CMOS circuits. Figure 4 illustrates a simplified cross section showing two transistors,​ one PMOS and one NMOS; these could be connected together as logic gates or as an analog amplifier or switch. The parasitic bipolar transistors responsible for latch-up behavior, Q<​sub>​1</​sub>​ (vertical PNP) and Q<​sub>​2</​sub>​ (lateral NPN) are as indicated. Since all these MOS devices are located close together on the monolithic die, with appropriate external excitation, the parasitic SCR devices may turn on, a behavior common with poorly designed CMOS circuits. Figure 4 illustrates a simplified cross section showing two transistors,​ one PMOS and one NMOS; these could be connected together as logic gates or as an analog amplifier or switch. The parasitic bipolar transistors responsible for latch-up behavior, Q<​sub>​1</​sub>​ (vertical PNP) and Q<​sub>​2</​sub>​ (lateral NPN) are as indicated.
Line 110: Line 110:
 Looking back at figure 1 we note that the triggering current is injected at the base of the NPN Q2. The ON state can just as eaisily be triggered by pulling a current out of the base of the PNP transistor Q1 as shown in figure 5. Looking back at figure 1 we note that the triggering current is injected at the base of the NPN Q2. The ON state can just as eaisily be triggered by pulling a current out of the base of the PNP transistor Q1 as shown in figure 5.
  
-The Programmable unijunction transistor or PUT is a close relative of other four layer devices in the thyristor family. Its has a four layered construction just like the SCR and has three terminals named anode(A), cathode(K) and gate(G) again like the thyristors. It is often reffered ​to as a programmable Uni-Junction Transistor because its characteristics and parameters are similar to those of the UJT. The programmablility ​of typical UJT parameters like intrinsic standoff ratio (η), peak voltage(Vp) etc is made by connecting two external resistors. In a conventional UJT, the parameters like Vp, η etc are fixed by the device processing and cannot be changed by the user. The main application of programmable UJT are relaxation oscillators , thyristor triggering, pulse circuits and timing circuits. ON Semiconductor® is the only manufacturer of PUTs today. ​ 2N6027 is the most common type number and it is available in a TO-92 plastic package. ​ The internal block diagram and circuit symbol of PUT are shown below.+The Programmable unijunction transistor or PUT is a close relative of other four layer devices in the thyristor family. Its has a four layered construction just like the SCR and has three terminals named anode(A), cathode(K) and gate(G) again like the thyristors. It is often referred ​to as a programmable Uni-Junction Transistor because its characteristics and parameters are similar to those of the UJT. The programmability ​of typical UJT parameters like intrinsic standoff ratio (η), peak voltage(Vp) etc is made by connecting two external resistors. In a conventional UJT, the parameters like Vp, η etc are fixed by the device processing and cannot be changed by the user. The main application of programmable UJT are relaxation oscillators , thyristor triggering, pulse circuits and timing circuits. ON Semiconductor® is the only manufacturer of PUTs today. ​ 2N6027 is the most common type number and it is available in a TO-92 plastic package. ​ The internal block diagram and circuit symbol of PUT are shown below.
  
 {{ :​university:​courses:​alm1k:​alm-lab-scr_f5.png?​600 |}} {{ :​university:​courses:​alm1k:​alm-lab-scr_f5.png?​600 |}}
university/courses/alm1k/alm-lab-scr.txt · Last modified: 27 May 2022 21:05 by Doug Mercer