This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
university:courses:alm1k:alm-lab-pv [10 Mar 2022 15:12] – [Hardware Setup:] Doug Mercer | university:courses:alm1k:alm-lab-pv [10 Mar 2022 15:12] (current) – [Hardware Setup:] Doug Mercer | ||
---|---|---|---|
Line 111: | Line 111: | ||
Set the voltage vertical scale of scope channel A to 0.5V/div. The current vertical scale of channel A will depend on the maximum current your panel can generate. | Set the voltage vertical scale of scope channel A to 0.5V/div. The current vertical scale of channel A will depend on the maximum current your panel can generate. | ||
- | Set the frequency of waveform generator A to 100 Hz, and the horizontal time base so that at least one full 0 to V< | + | Set the frequency of waveform generator A to 100 Hz, and the horizontal time base so that at least one full 0 to V< |
With the channel A generator disabled (in Hi-Z Mode), first measure the open circuit voltage produced by the panel when in full sun light. Set the Max voltage | With the channel A generator disabled (in Hi-Z Mode), first measure the open circuit voltage produced by the panel when in full sun light. Set the Max voltage |