This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:courses:alm1k:alm-lab-4s [14 Nov 2016 16:46] – [Switches in Parallel:] Doug Mercer | university:courses:alm1k:alm-lab-4s [03 Nov 2021 20:32] (current) – [Activity: BJT device as a switch] Doug Mercer | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ======Activity | + | ======Activity: |
=====Objective: | =====Objective: | ||
Line 78: | Line 78: | ||
====Switches in Parallel: | ====Switches in Parallel: | ||
- | Two NPN transistors can be connected with their collectors and emitters in parallel, figure3, which provides a way to switch on the load from two different signals. Either input can turn on the load but both need to be off for the load to be off. This is referred to as an “OR” function. | + | Two NPN transistors can be connected with their collectors and emitters in parallel, figure3, which provides a way to switch on the load from two different signals. Either input can turn on the load but both need to be off for the load to be off. This is referred to as an “OR” |
{{ : | {{ : | ||
Line 107: | Line 107: | ||
Again, set PIO 0 and PIO 1 to all four combinations of logic 0 and 1. Note which combinations turn on the LED. The voltage at the LED and Q< | Again, set PIO 0 and PIO 1 to all four combinations of logic 0 and 1. Note which combinations turn on the LED. The voltage at the LED and Q< | ||
+ | |||
+ | **Resources: | ||
+ | |||
+ | * LTSpice files: [[downgit> | ||
+ | * Fritzing files: [[downgit> | ||
**For Further Reading:** | **For Further Reading:** | ||
- | http:// | + | [[wp>Transistor|Transistor]]\\ |
- | https:// | + | [[wp>Light-emitting_diode|Light- emitting diode]]\\ |
- | https:// | + | [[wp>LED_circuit|LED circuit]] |
- | **Return to ALM Lab Activity [[university: | + | **Return to [[university: |
+ | **Return to [[university: | ||
+ | **Return to Electronics | ||