Wiki

This version is outdated by a newer approved version.DiffThis version (08 Jan 2018 15:10) is a draft.
Approvals: 0/1
The Previously approved version (13 Apr 2015 17:27) is available.Diff

This is an old revision of the document!


Activity 4: BJT Characteristic Curves

Objective:

The purpose of this activity is to investigate the collector current, IC vs. collector voltage, VCE characteristics of the BJT. The ADALP2000 kit of parts will contain a number of transistors, both NPN and PNP devices of various types, that can be used.

Notes:

As in all the ALM labs we use the following terminology when referring to the connections to the M1000 connector and configuring the hardware. The green shaded rectangles indicate connections to the M1000 analog I/O connector. The analog I/O channel pins are referred to as CA and CB. When configured to force voltage / measure current -V is added as in CA-V or when configured to force current / measure voltage -I is added as in CA-I. When a channel is configured in the high impedance mode to only measure voltage -H is added as CA-H.

Scope traces are similarly referred to by channel and voltage / current. Such as CA-V , CB-V for the voltage waveforms and CA-I , CB-I for the current waveforms.

Background:

The variable analog outputs supplied by the ALM1000 hardware are voltages but can also measure current at same time. The Bipolar Junction Transistor can be modeled as a current controlled current source. The BJT collector current, IC, is controlled by the much smaller base current, IB. The generator output voltage must be converted into a suitable small current to drive the base terminal of the device under investigation. A simple high value resistor can be used to convert this voltage into a current, as shown in figure 1. However, only if the voltage across the resistor is known or controlled in some way. In this simple circuit, the base current IB = (CB-V - VBE)/10KΩ. We can set CB-V to known values but we don't know the exact value of VBE. We can of course remove an estimate of the VBE mathematically. This is still only an estimate but close enough for our purposes here.

Figure 1 NPN IC vs. VCE characteristic curve measurements

If we sweep the voltage on the collector, VCE, while changing the voltage on the resistor in a step wise fashion for each sweep cycle of the collector voltage, we can generate a set of characteristic curves of the collector current vs collector emitter voltage for a set of base currents.

Materials:

ADALM1000 Hardware module
Solder-less Breadboard
1 - 10KΩ Resistor
1 - small signal NPN transistor (2N3904, SSM2212)

NPN device Directions:

Build the simple characteristic curve measurement circuit shown in figure 1 on your solder-less breadboard. The green boxes indicate where to connect the M1000.

Hardware Setup:

Set the Channel B generator output to the 10 level stair-step waveform. Set the frequency to 20Hz, the Max to 4.6 V and the Min to 0.6 V. The extra 0.6 volts is an initial estimate of VBE. The waveform in the display should start at 0.6V and increase in 0.4 V increments to 4.6 V. Set the channel A generator to a triangle wave with a Max of 5.0 V and a Min of 0 V (wave should swing from 0 to 5V). Set the frequency to 200 Hz ( 10 times the 20 Hz of channel B). Comparing the waveforms in channel A and channel B, the triangle wave in channel A should go through one cycle from 0 to 5 V and back to zero during the time of one step in the waveform in channel B. Adjust the phases of channel A and/or channel B to make them line up in this way if they do not.

Procedure:

The 0.4 V steps in the voltage driving the 10 KΩ base resistor will produce approximately 0.4 V/10 KΩ or 40 uA steps in the base current. Using the scope in XY mode plot channel CA-V on the horizontal axis (VCE) and channel CA-I (IC) on the vertical axis. You should see a set of 10 curves of IC vs. VCE, one for each of the 10 different base current levels. These base current levels should be approximately 0, 40uA, 80uA, 120uA … 360uA. It may be necessary to slightly adjust the 0.6V offset level of the first step of channel B up or down slightly to insure it is right at the initial turn on value ( IB=0 and IC=0) of the transistor you are testing.

Questions:

From the measured data calculate the current gain Beta ( ß=IC/IB ) for each device.
Using the curve for the highest base current step, calculate the early voltage (VA) for each device.
Calculate the Beta Early voltage product ( ß*VA) for each device.
Compare your results with manufacturer specifications for each device measured.

PNP device Directions:

To measure the PNP device, alter the characteristic curve measurement circuit as shown in figure 2. The connections are not very different but the polarity of the voltage waveforms generated by channel A and channel B must now be negative with respect to the PNP emitter. To accommodate this the emitter is now connected to +5 V.

You can use the same step staircase waveform you used for the NPN device to drive the base current for the PNP device. However, you will need to set the Max to +5 V - VBE or 4.4 V and set the Min to 0.4 V. The waveform in the display should now start at 4.4 V and decrease in 0.4 V increments to 0.4 V. The channel A triangle wave can have the same 5.0 V Max and 0 V Min. Check to make sure that the triangle wave in channel A goes through one cycle from 5 V to 0 and back to 5 V during the time of one step in the waveform in channel 2. Change the phase of channel A and/or B as necessary.

Figure 2 PNP IC vs. VCE characteristic curve measurments

Questions:

Again, from the measured data calculate the current gain Beta ( ß=IC/IB ) for each device.
Using the curve for the highest base current step, calculate the early voltage (VA) for each device.
Calculate the Beta Early voltage product ( ß*VA) for each device.
Compare your results with manufacturer specifications for each device measured.

For Further Reading:

http://en.wikipedia.org/wiki/Bipolar_junction_transistor
http://www.physics.csbsju.edu/trace/NPN.CC.html

Return to ALM Lab Activity Table of Contents

university/courses/alm1k/alm-lab-4.1515420638.txt.gz · Last modified: 08 Jan 2018 15:10 by Doug Mercer