This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
university:courses:alm1k:alm-lab-28 [25 Sep 2019 20:08] – [Making a SPDT Analog Switch with the CD4007 transistor array] Doug Mercer | university:courses:alm1k:alm-lab-28 [17 Jan 2021 19:46] – [Making a SPDT Analog Switch with the CD4007 transistor array] Doug Mercer | ||
---|---|---|---|
Line 138: | Line 138: | ||
=====Making a SPDT Analog Switch with the CD4007 transistor array===== | =====Making a SPDT Analog Switch with the CD4007 transistor array===== | ||
- | In addition to an analog SPDT switch this configuration is often called a pass gate or 2 into 1 MUX (multiplexer). The configuration is shown in figure 11. | + | In addition to an analog SPDT switch this configuration is often called a pass or transmission |
{{ : | {{ : | ||
Line 148: | Line 148: | ||
**For Further Reading:** | **For Further Reading:** | ||
+ | {{ : | ||
[[wp> | [[wp> | ||
[[wp> | [[wp> | ||
[[wp> | [[wp> | ||
[[wp> | [[wp> | ||
- | [[wp> | + | [[wp> |
+ | [[wp> | ||
**Return to Lab Activity [[university: | **Return to Lab Activity [[university: | ||