To investigate simple push-pull or class B amplifier output stage examples.
As in all the ALM labs we use the following terminology when referring to the connections to the M1000 connector and configuring the hardware. The green shaded rectangles indicate connections to the M1000 analog I/O connector. The analog I/O channel pins are referred to as CA and CB. When configured to force voltage / measure current -V is added as in CA-V or when configured to force current / measure voltage -I is added as in CA-I. When a channel is configured in the high impedance mode to only measure voltage -H is added as CA-H.
Scope traces are similarly referred to by channel and voltage / current. Such as CA-V , CB-V for the voltage waveforms and CA-I , CB-I for the current waveforms.
The role of an output stage is to provide power gain. It should have high input impedance and low output impedance. An obvious choice for this stage is the emitter follower. However, in order to provide both current sourcing and sinking capabilities, two complementary followers are needed, an NPN type to source current and a PNP type to sink current. The result is known as the push-pull configuration, of which figure 1 shows a simple configuration. Here R1 and R2 are used to sense the collector currents of Q1 and Q2, as well as to limit these currents in case of output overloading.
ADALM1000 hardware module
Solder-less breadboard and jumper wire kit
2 - 100 Ω resistors
1 - 2.2 KΩ resistor
2 - 10 KΩ resistors
2 - NPN transistors ( 2N3904 or SSM2212 )
2 - PNP transistors ( 2N3906 or SSM2220 )
Before starting make sure the power supplies from the ALM1000 hardware are disconnected from the breadboard. The circuit and the connections to the Lab hardware are as indicated in figure 1. The channel B Hi-Z mode input CB-H should to be connected to the junction of Q1 and Q2 emitters.
Figure 1 Push - Pull Output stage
The channel A voltage generator, CA-V, should be configured for a 100 Hz sine wave with 2.0 volt Min value and 3.0 volt Max value.
Next, apply power and adjust the voltage generator so that CA-V is a 100 Hz triangle wave. Use the oscilloscope in the x-y mode to observe the voltage-transfer curve of the circuit. Save the curve to a .csv or .eps file for inclusion in your lab report, label all breakpoints, slopes, and saturation levels, and justify them in terms of circuit operation and given component values.
Switch the scope to the time display mode, and adjust the waveform generator so that CA-V is a 100 Hz sine wave with the Min and Max values both equal to 2.5 V.
Gradually increase the amplitude of the sine wave, keeping it centered on 2.5 V, until you just begin to see an signal on scope channel B appear at the output. For what range of amplitude values of CA-V can we say that both Q1 and Q2 are essentially off? Confirm this by observing the voltages of the current-sensing resistances R1 and R2.
Lower the CA-V Min value to 1V, and raise the Max value to 4 V. Record the P-P amplitude of the output waveform as well as the collector currents of Q1 and Q2, which can be found from the voltages across R1 and R2, and justify your findings in terms of circuit operation and the given component values.
Repeat, but with CA-V Min value lowered to 0 V and Max value raised a 5 V; and comment.
Simulate the circuit of figure 1 using ADIsimPE (or SIMetrix), compare with your lab findings, and justify any differences.
Add questions here.
The large amount of distortion at the zero-crossings in the basic push-pull stage of figure 1 is a result of a dead zone when both the NPN and PNP emitter followers are off. The waveform's dead zone at the zero-crossings is dramatically reduced if we pre-bias the BJTs with two VBE drops, as shown in figure 2. Here, the pre-bias function is provided by diode connected NPN Q1 and PNP Q3. Resistors R1 and R2 provide bias current and set the idle current that flows in the output devices Q2 and Q4.
With the power disconnected, assemble the circuit of figure 2, keeping leads as short and neat as possible. NPN transistors Q1 and Q2, PNP transistor Q3and Q4 should be selected from the available devices with the best matching of VBE. Transistors fabricated in the same package such as the SSM2212 or the CA3046 tend to match much better than individual devices.
Figure 2 Push - pull output stage with zero-crossing distortion elimination.
Use the same hardware setup as you did for the circuit in figure 1.
If we examine figure 2, the loop formed by the base emitter voltages of Q1, Q2, Q3 and Q4 we know that the sum of the voltage drops around the loop must sum to zero. Thus if Q1 is identical to Q2 and Q3 is identical to Q4, the voltage around the loop will be zero only when the current in Q1 is identical to the current in Q2 and the current in Q3 is identical to the current in Q4. Thus when the output is at 2.5 volts i.e. there is no current in RL, the input must also be at 2.5 volts.
Use the oscilloscope in the X-Y mode to observe the voltage-transfer curve of the circuit. Save the curve to a .csv or .eps file for inclusion in your lab report, label all breakpoints, slopes, and saturation levels, and justify them in terms of circuit operation and given component values.
Display the input / output transfer curve of the circuit of figure 2, save the date to a .csv file or save the cures to a .eps file, label all breakpoints, slopes, and saturation levels. In your lab report justify them in terms of circuit operation and the given component values.
Apply a 100 Hz sine wave centered on 2.5 V offset and various amplitudes, and verify that the circuit yields Vout ? Vin all the way down to small amplitudes. What is the upper limit on the amplitude of CA-V before the circuit starts to distort? Justify quantitatively in terms of the transfer curve just observed.
Using your scope input, measure Vout as well as the voltage across R3 and R4 for the following DC values of Vin: 1 V, 2 V, 2.5 V, 3 V, 4 V. Then, tabulate Vout and the current in RL as well as the collector currents of Q2 and Q4 and comment. Use the DC shape of the voltage generator to set the DC value.
Measure the input impedance by inserting a 10 KΩ resistor in series with the signal generator (between CA-V and the emitters of Q1and Q3) and connecting the channel B Hi-Z input at the emitter of Q1. Use the CA-V - CB-V Math waveform to display the voltage across the 10 KΩ resistor. Capture the input current vs. the input voltage and calculate the input resistance from the slope of the curve. Justify your results based on the component values used in the circuit.
Simulate the circuit of figure 2 using ADIsimPE (or SIMetrix), compare with your lab findings, and justify any differences.
Remembering the loop formed by the base emitter voltages of Q1, Q2, Q3 and Q4 we also know that the order of the voltage drops around the loop can be interchanged. So if we interchange the VBE's of NPN Q1 and PNP Q3 we get the configuration shown in figure 3. This arrangement is sometime referred to as a “diamond buffer” because of the shape formed by the four emitter / base connections. Some of you may recognize the combination of Q3 and Q2 as the low offset follower we discussed earlier in the lab section on emitter followers. The circuit uses the VBE shift up of a PNP emitter follower to partially cancel the VBE shift down of an NPN emitter follower. Transistors Q1 and Q4 are simply the complement of Q3 and Q2.
Figure 3 Emitter follower zero-crossing distortion elimination
Use the same hardware setup as you did for the circuit in figure 2.
Display the input / output transfer curve of the circuit of figure 3, save the date to a .csv file or save the cures to a .eps file, label all breakpoints, slopes, and saturation levels, and justify them in terms of circuit operation and the given component values. How do they compare to the circuit in figure 2?
Apply a 100 Hz sine wave centered on 2.5 V and various amplitudes, and verify that the circuit yields Vout ? Vin all the way down to small amplitudes. What is the upper limit on the amplitude of CA-V before the circuit starts to distort? Justify quantitatively in terms of the transfer curve just observed.
Using your scope input, measure Vout as well as the voltage across R3 and R4 for the following DC values of Vin: 1V, 2V, 2.5 V, 3 V, 4 V. Then, tabulate Vout and the current in RL as well as the collector currents of Q2 and Q4 and comment. Use the DC shape of the CA generator to set the DC value.
Measure the input impedance by inserting a 10 KΩ resistor in series with the signal generator (between CA-V and the bases of Q1and Q3) and connect the channel CB-H scope to measure the voltage across the 10 KΩ resistor as you did for the circuit in figure 3. Capture the input current vs. the input voltage and calculate the input resistance from the slope of the curve. Justify your results based on the component values used in the circuit. How do your results compare to what you measured for the circuit in figure 2?
Simulate the circuit of figure 3 using ADIsimPE (or SIMetrix), compare with your lab findings, and justify any differences.
In figure 4 we see another slight variation on the circuit in figure 3. Since the aim of these output stages id to provide an output voltage that is ideally identical to the input, transistors Q1 and Q2 can be thought of as being “diode” connected similar to the arrangement in figure 2 but with the NPN and PNP interchanged. This will not be exactly the case in real life so there will be a small error current flowing back into the emitters of Q2 and Q4 based on any mismatches between the devices.
Figure 4 Push-Pull output stage version 4
Repeat the same test you performed on the figure 2 and figure 3 circuits on the circuit in figure 4.
For Further Reading:
Push-Pull Output
Increase amplifier output drive using a push-pull stage
Return to Lab Activity Table of Contents