This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
software:linux:docs:iio:iio [30 May 2012 13:36] – [IIO Ring Buffer] Michael Hennerich | software:linux:docs:iio:iio [03 Jan 2013 20:42] – external edit | ||
---|---|---|---|
Line 44: | Line 44: | ||
* These are similar to input in that they provide a route to user space for hardware triggered events. Such events include threshold detectors, free-fall detectors and more complex action detection. | * These are similar to input in that they provide a route to user space for hardware triggered events. Such events include threshold detectors, free-fall detectors and more complex action detection. | ||
- | <note> | + | <WRAP round help> |
A given device may have one or more event channel. | A given device may have one or more event channel. | ||
- | </note> | + | </WRAP> |
* Hardware ring buffer support | * Hardware ring buffer support |